cancel
Showing results for 
Search instead for 
Did you mean: 

Precise Motion Control for BLDC Motor

Youni
Associate II

Hi,

 

I have following Harware configuration:

 

- X-NUCLEO-IHM16M1 (STSPIN830)

-  NUCLEO-L476RG

 

BLDC Motor with three analog hall sensors

 

I'd like to be able to configure your Motor workbench to do the job.

 

Questions:

-   Are the boards X-NUCLEO-IHM16M1 + NUCLEO-L476RG compatible ? I suppose yes

-   How  would you configure position control for analog Hall sensor with your motorworkbench ?

 

Do you have any api or docs which might help ?

Many thanks

Younes

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
GMA
ST Employee

Hello @Youni,

Please, refer to the position control application note.
As mentioned, this feature is only available with a PMSM motor with quadrature encoder (with index signal).
APIs are also described.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA