STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1725 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4873 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9558 Views
  • 5 replies
  • 3 kudos

Resolved! STM32G4 - XCUBE-DPOW

Good day,we are currently integrating the XCUBE-Dpow library but are running into multiple issues due to the lack of code documentation of the library.- We are not using HTIM Channel-C but -D. After changing multiple entries in the template files of ...

JuculianD_0-1727782220410.png

Resolved! evspin32f0602s1 motor driving

Hello, I am very new for ST MCU,I have made may own evspin32f0602s1 board , after many trial and errors also after gone through documentation  ,I got  PWM output. but problem is that I  getting it at Reserved pins of MCU (TP1,TP2,TP3 in evolution boa...

KVijay32 by Associate II
  • 8766 Views
  • 15 replies
  • 0 kudos

Resolved! Remap PWM Pins

Hello, I am using MCSDK_v6.3.1 and encountered a problem when changing TIM1 PWM pins:I cloned B-G431B-ESC1 Devkit Inverter.I changed High Side TIM1 PWM pinsUH: PA8 -> PC2VH: PA9 -> PC1WH: PA10 -> PC0When I now want to create a project with the modifi...

c_dev05 by Associate III
  • 1107 Views
  • 1 replies
  • 0 kudos

Software support for motor control

Hi Guys,I am new to motor control, and I have chosen STs controller board NUCLEO-G431RB and inverter board X-NUCLEO-IHM08M1 for BLDC motor control. please give me an insight on what all software tools you provide for easy development. Is there any to...

Difference between NOMINAL_CURRENT and IQMAX

I need to implement runtime current limitation.Another thread says to use "PID_SetUpperOutputLimit" on the PidSpeedHandle for that to change the values originally defined by IQMAX, which makes sense.However, I also found NOMINAL_CURRENT used for MaxP...

DMeie.2 by Senior II
  • 1040 Views
  • 0 replies
  • 0 kudos

P-NUCLEO-IHM03

Hi,Starting from this development board, would like to know if I can add easily encoder (which one) and if there are example project for a servo driver, I mean code to control speed and position of the gimbal motor.Thanks in advance

FMarr.2 by Associate III
  • 1845 Views
  • 2 replies
  • 0 kudos