cancel
Showing results for 
Search instead for 
Did you mean: 

EVSPIN32F0251 board PA0 Pin Use

PPate.2
Associate III

Hello ,

 I have STSPIN32F0251 Development Board. In that board schematic we have found PA0_B Label that is connected default to Pin No 12 (PA0) of MCU(STSPIN32F251) .

we want to know the importance and reason of connecting it. also where in firmware code it is defined and used.

same for PA1_B and PA2_B pins also.

we are using keil IDE and Motor Control Workbench Generated Code with MCSDK 5.4.6 version

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Gael A
ST Employee

Hello PPate.2,

The PA0_B, PA1_B and PA2_B are used for 6-STEP BEMF sensing. Therefore it is useless in FOC and can be rerouted for Hall Sensors or OverVoltage protection thanks to PA0_Hall or PA0_B_VN.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.

View solution in original post

1 REPLY 1
Gael A
ST Employee

Hello PPate.2,

The PA0_B, PA1_B and PA2_B are used for 6-STEP BEMF sensing. Therefore it is useless in FOC and can be rerouted for Hall Sensors or OverVoltage protection thanks to PA0_Hall or PA0_B_VN.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.