STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using queue from a C++ class running in a ThreadX thread causes task to overflow memory. Bug? (workaround exists)

STM32L5x2xx processor.STM32CubeIDEVersion: 1.10.1Build: 12716_20220707_0928 (UTC)Program structure:Main.c calls CPP_LINK (a C++ routine) that enables system level drivers (with ThreadX mutexes), then starts main ThreadX task.C++ classes own ThreadX o...

Handling UART errors in HAL

I am struggling to establish robust UART communication using HAL. It also seems I am not alone, there were many similar questions here, all closed without an answer. Here are some of them:https://community.st.com/s/question/0D50X00009XkfAH/handling-u...

maple by Associate II
  • 6145 Views
  • 4 replies
  • 0 kudos

Linker script specifies .TxDescripSection > Memory_B2 but .TxDescripSection ends up in RAM section (LwIP_HTTP_Server_Netcoon_RTOS on STMF767zi)

Hello,The linker script in the demo example specifies:/* Specify the memory areas */ MEMORY { FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 499K Memory_B1(xrw) : ORIGIN = 0x2007C000, LENGTH = ...

0693W00000QLAPMQA5.png
Johi by Senior III
  • 4930 Views
  • 6 replies
  • 1 kudos

Ethernet MAC, TCP Checksum offload stops working

Hi,I'm trying to push through a lot of data over Ethernet using TCP. It's working for a while and then the TCP checksums disappear, IPv4 checksums are still there. This happens after 1-2MB -> 25GB depending if there's a python or C client on the PC, ...

LKert by Associate
  • 7085 Views
  • 11 replies
  • 1 kudos

M4 core heap issue on STM32H745.

I am working on STM32H745 discovery board. I have the following peripherals configured on both cores-Cortex M4- FreertosCortex M7- Freertos, Ethernet, LWIP, USART, QSPI, SDRAM.In M4 core there is a default task in which LED is blinking. When I enable...

Akast.2 by Associate II
  • 1568 Views
  • 1 replies
  • 0 kudos