cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F723VCT USB host msc design using stm32cubeIDE 1.5 with middle ware example

Wzhan.6
Associate

follow youtube STM32 USB training - 11.2 USB MSC host labs to try a board with STM32F723vct6.

set as USB Host_Only on HS

static void USBH_UserProcess (USBH_HandleTypeDef *phost, uint8_t id)

{

 /* USER CODE BEGIN CALL_BACK_1 */

 switch(id)

 {

 case HOST_USER_SELECT_CONFIGURATION:

 break;

 case HOST_USER_DISCONNECTION:

 Appli_state = APPLICATION_DISCONNECT;

 break;

 case HOST_USER_CLASS_ACTIVE:

 Appli_state = APPLICATION_READY;

 break;

 case HOST_USER_CONNECTION:

 Appli_state = APPLICATION_START;

 //---------------zz

 if (f_mount (&USBH_fatfs, USBHPath, 0) != FR_OK )

 {

//     Display_Line8x6 (1, 0, "fmout fail", 15,nH_lit);

 }else {

//     Display_Line8x6 (1, 0, "fmout rdy", 15,nH_lit);

//

 }

f_mout can detect thumb drive plug in/plug out but never go to Appli_state == APPLICATION_READY

but can be OK If try on STM32F723E-DISCO board, can create files on thumb drive and save text to file

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Wzhan.6
Associate

issue resolved, it is USB A signal D+/D- swapped.

View solution in original post

1 REPLY 1
Wzhan.6
Associate

issue resolved, it is USB A signal D+/D- swapped.