STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! mbedTLS client example STM32Cube_FW_F7_V1.17.0

Hi, I'm running the following example project:STM32Cube_FW_F7_V1.17.0\Projects\STM32F769I-Discovery\Applications\mbedTLS\SSL_Clienton the development board STM32F769I-Discovery.Seems like the application uses the .h file STM32Cube_FW_F7_V1.17.0\Middl...

Jonas_A by Associate II
  • 995 Views
  • 1 replies
  • 0 kudos

Resolved! Migrating project from Nucleo to custom board

Hi,I've a project that has quite a lot of peripheral configurations, plus code, based around Nucleo H755.Now I need to port this into a new project based on the same chip (STM32H755ZIT6) but targeting my own board design. I will be using the same per...

bramble by Senior
  • 1086 Views
  • 2 replies
  • 0 kudos

Should DMA variables be volatile

I am using the DMA in a few places. I am wondering should these variables be volatile. As it is, the compiler has no idea when the data will be read from or written into these variables. When that is the case, shouldn't you make the variable volatile...

Carl_G by Senior III
  • 4780 Views
  • 14 replies
  • 9 kudos

HAL_FLASHEx_Erase() – STM32L072

Hi STM32 Community,I'm working with the STM32L072 MCU which has 192KB of Flash. I'm implementing a bootloader + dual app OTA architecture. Here's my current memory layout:Region Start Address End Address DescriptionBootloader0x080000000x08002FFFStati...