Skip to main content
KKjel.1
Senior
August 19, 2024
Solved

How to stop debug messages in lwIP?

  • August 19, 2024
  • 6 replies
  • 2068 views

Hi

I have a project using lwIP, created by STM32Cube.

It works fine, but I really want to shut OFF the debug messages.

I have searched and tried a bunch of different things, but nothing seems to be able to stop it.

 

Example of error/debug message: "netif is not up, old style port?" failed at line 744 in C:\..."

 

Thanks 

This topic has been closed for replies.
Best answer by Passerby

Add a global macro definition " LWIP_NOASSERT"

6 replies

ST Employee
August 19, 2024

Hello @KKjel.1,

Could you please verify that you don't have any debug macros enabled in the lwipopts.h file? This might be the reason for the debug messages you are seeing.

 

With Regards,

"If your question is answered, please close this topic by clicking ""Accept as Solution""."
KKjel.1
KKjel.1Author
Senior
August 19, 2024

There is no DEBUG macros in that file.

Here is the complete file:

 

/* USER CODE BEGIN Header */
/**
******************************************************************************
* File Name : lwipopts.h
* Description : This file overrides LwIP stack default configuration
* done in opt.h file.
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */

/* Define to prevent recursive inclusion --------------------------------------*/
#ifndef __LWIPOPTS__H__
#define __LWIPOPTS__H__

#include "main.h"

/*-----------------------------------------------------------------------------*/
/* Current version of LwIP supported by CubeMx: 2.1.2 -*/
/*-----------------------------------------------------------------------------*/

/* Within 'USER CODE' section, code will be kept by default at each generation */
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

#ifdef __cplusplus
extern "C" {
#endif

/* STM32CubeMX Specific Parameters (not defined in opt.h) ---------------------*/
/* Parameters set in STM32CubeMX LwIP Configuration GUI -*/
/*----- WITH_RTOS enabled (Since FREERTOS is set) -----*/
#define WITH_RTOS 1
/*----- CHECKSUM_BY_HARDWARE enabled -----*/
#define CHECKSUM_BY_HARDWARE 1
/*-----------------------------------------------------------------------------*/

/* LwIP Stack Parameters (modified compared to initialization value in opt.h) -*/
/* Parameters set in STM32CubeMX LwIP Configuration GUI -*/
/*----- Value in opt.h for LWIP_DHCP: 0 -----*/
#define LWIP_DHCP 1
/*----- Default value in ETH configuration GUI in CubeMx: 1524 -----*/
#define ETH_RX_BUFFER_SIZE 1536
/*----- Default Value for LWIP_DNS: 0 ---*/
#define LWIP_DNS 1
/*----- Value in opt.h for MEM_ALIGNMENT: 1 -----*/
#define MEM_ALIGNMENT 4
/*----- Default Value for H7 devices: 0x30044000 -----*/
#define LWIP_RAM_HEAP_POINTER 0x30000200
/*----- Value supported for H7 devices: 1 -----*/
#define LWIP_SUPPORT_CUSTOM_PBUF 1
/*----- Value in opt.h for LWIP_ETHERNET: LWIP_ARP || PPPOE_SUPPORT -*/
#define LWIP_ETHERNET 1
/*----- Value in opt.h for LWIP_DNS_SECURE: (LWIP_DNS_SECURE_RAND_XID | LWIP_DNS_SECURE_NO_MULTIPLE_OUTSTANDING | LWIP_DNS_SECURE_RAND_SRC_PORT) -*/
#define LWIP_DNS_SECURE 7
/*----- Value in opt.h for TCP_SND_QUEUELEN: (4*TCP_SND_BUF + (TCP_MSS - 1))/TCP_MSS -----*/
#define TCP_SND_QUEUELEN 9
/*----- Value in opt.h for TCP_SNDLOWAT: LWIP_MIN(LWIP_MAX(((TCP_SND_BUF)/2), (2 * TCP_MSS) + 1), (TCP_SND_BUF) - 1) -*/
#define TCP_SNDLOWAT 1071
/*----- Value in opt.h for TCP_SNDQUEUELOWAT: LWIP_MAX(TCP_SND_QUEUELEN)/2, 5) -*/
#define TCP_SNDQUEUELOWAT 5
/*----- Value in opt.h for TCP_WND_UPDATE_THRESHOLD: LWIP_MIN(TCP_WND/4, TCP_MSS*4) -----*/
#define TCP_WND_UPDATE_THRESHOLD 536
/*----- Value in opt.h for LWIP_NETIF_LINK_CALLBACK: 0 -----*/
#define LWIP_NETIF_LINK_CALLBACK 1
/*----- Value in opt.h for TCPIP_THREAD_STACKSIZE: 0 -----*/
#define TCPIP_THREAD_STACKSIZE 1024
/*----- Value in opt.h for TCPIP_THREAD_PRIO: 1 -----*/
#define TCPIP_THREAD_PRIO 24
/*----- Value in opt.h for TCPIP_MBOX_SIZE: 0 -----*/
#define TCPIP_MBOX_SIZE 6
/*----- Value in opt.h for SLIPIF_THREAD_STACKSIZE: 0 -----*/
#define SLIPIF_THREAD_STACKSIZE 1024
/*----- Value in opt.h for SLIPIF_THREAD_PRIO: 1 -----*/
#define SLIPIF_THREAD_PRIO 3
/*----- Value in opt.h for DEFAULT_THREAD_STACKSIZE: 0 -----*/
#define DEFAULT_THREAD_STACKSIZE 1024
/*----- Value in opt.h for DEFAULT_THREAD_PRIO: 1 -----*/
#define DEFAULT_THREAD_PRIO 3
/*----- Value in opt.h for DEFAULT_UDP_RECVMBOX_SIZE: 0 -----*/
#define DEFAULT_UDP_RECVMBOX_SIZE 6
/*----- Value in opt.h for DEFAULT_TCP_RECVMBOX_SIZE: 0 -----*/
#define DEFAULT_TCP_RECVMBOX_SIZE 6
/*----- Value in opt.h for DEFAULT_ACCEPTMBOX_SIZE: 0 -----*/
#define DEFAULT_ACCEPTMBOX_SIZE 6
/*----- Value in opt.h for RECV_BUFSIZE_DEFAULT: INT_MAX -----*/
#define RECV_BUFSIZE_DEFAULT 2000000000
/*----- Value in opt.h for LWIP_STATS: 1 -----*/
#define LWIP_STATS 0
/*----- Value in opt.h for CHECKSUM_GEN_IP: 1 -----*/
#define CHECKSUM_GEN_IP 0
/*----- Value in opt.h for CHECKSUM_GEN_UDP: 1 -----*/
#define CHECKSUM_GEN_UDP 0
/*----- Value in opt.h for CHECKSUM_GEN_TCP: 1 -----*/
#define CHECKSUM_GEN_TCP 0
/*----- Value in opt.h for CHECKSUM_GEN_ICMP6: 1 -----*/
#define CHECKSUM_GEN_ICMP6 0
/*----- Value in opt.h for CHECKSUM_CHECK_IP: 1 -----*/
#define CHECKSUM_CHECK_IP 0
/*----- Value in opt.h for CHECKSUM_CHECK_UDP: 1 -----*/
#define CHECKSUM_CHECK_UDP 0
/*----- Value in opt.h for CHECKSUM_CHECK_TCP: 1 -----*/
#define CHECKSUM_CHECK_TCP 0
/*----- Value in opt.h for CHECKSUM_CHECK_ICMP6: 1 -----*/
#define CHECKSUM_CHECK_ICMP6 0
/*-----------------------------------------------------------------------------*/
/* USER CODE BEGIN 1 */

#define DNS_MAX_TTL 0
#define DNS_MAX_SERVERS 3

/* USER CODE END 1 */

#ifdef __cplusplus
}
#endif
#endif /*__LWIPOPTS__H__ */

PasserbyBest answer
Associate III
August 19, 2024

Add a global macro definition " LWIP_NOASSERT"

KKjel.1
KKjel.1Author
Senior
August 19, 2024

Thanks, Passerby, nice and easy, and it works !

 

Kaare

Associate III
August 19, 2024

"netif is not up, old...." is a error message , you should pay attention to that.

Not printf does not mean that errors disappear