STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

diode

HelIo,I connected the anode from a diode to the operating voltage and the cathode to a pinx. I need ground to make the diode glow.  How can this be implemented?

Sax by Associate III
  • 5301 Views
  • 13 replies
  • 0 kudos

Resolved! Stm32f042f6 - 'funny' problem with programming

Hi! Just as a comment, did anyone had that kind of problem?uC is not found or easily losing connection while erase/program.Everything is properly designed and soldered (even programmer pins are temp. soldered to board).Every connection was checked an...

oeliks by Senior
  • 5407 Views
  • 11 replies
  • 6 kudos

NUCLEO H743, troubles with ADC and LWIP

Hello,I am currently working on a project involving transferring data acquired with an ADC through ethernet.Im am using the STM32H743 MCU.I have been building small projects using LWIP, and was able to connect to the board, ping and transmit some arr...

GLeje.2 by Associate II
  • 2238 Views
  • 4 replies
  • 0 kudos

Resolved! Custom STM32 Nucleo 64 PCB without CN2

I am in the  process of designing a custom PCB board that uses the CN4 ST-link pins to flash to the processor (rather than the standard USB Micro-B connector). Through testing with a multimeter, I have confirmed that the CN4 line is connected to the ...