Nucleo STM32F411RE, two VL53L0X, a DRV8833 driver and 2 6v motors. Power is from 2 x 3.7v18650 batteries (7.4v) on the VIN power input.5v regulator powers the 2 sensors.The batteries power the regulator, the VIN of the board and the motor driver.I do...