Skip to main content
_richard
Associate III
June 6, 2023
Solved

SWO also on CS of a SPI EEPROM is safe/state of the art?

  • June 6, 2023
  • 4 replies
  • 1755 views

i got schematics for a board that i should work on. it's stm32 L0 based.

they did put SWO also on CS of a SPI EEPROM. I'm not a hardware designer / debug protocol specialist but i could imagine debug scenarios where toggling the chip select of an EEPROM while debugging leads to unexpected results.

Would you say that putting SWO also on CS of a SPI EEPROM is safe / state of the art?

This topic has been closed for replies.
Best answer by Peter BENSCH

No problem - everyone stumbles across a misleading term or other inconsistency once in a while.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

4 replies

Peter BENSCH
ST Technical Moderator
June 6, 2023

Which STM32L0 do you have that has a SWO output?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Pavel A.
June 6, 2023

These days... they call art a rotten banana stuck on a wall. Who knows.

_richard
_richardAuthor
Associate III
June 6, 2023

that's a good question.

they did label pb3 at the stm32l072 as SWO, as well as the pin 6 at tag connect, and then they have pb3 also labelled as cs_ee at another sheet.

after your question i looked into the l072 manual and found that it has no SWO -> the labeling is wrong.

well, I'm not a hardware designer and try to work based on the info i get

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
June 6, 2023

No problem - everyone stumbles across a misleading term or other inconsistency once in a while.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.