MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

H3LIS332DL Interrupt events

Posted on October 23, 2013 at 11:48As Interrupt sources, what means the ''X/Y/Z High Event'' or ''... LOW Event'' in the datasheet? Are there defined trigger values for these events, and are they changeable in some registers? #h3lis331dl #acceler...

hmai by Associate
  • 1086 Views
  • 1 replies
  • 0 kudos

Finding land pattern for LIS3DH

Posted on October 22, 2013 at 16:32Hi,Where are the land patterns for LIS3DH, LLGA16 (3x3x1.0) 7983231 filed?I have tried searching for all of the above keywords but still come up empty handed, the closest i get is a land pattern by maxim, 90-0396.T...

interrupt generation problem during CTRL_REG3 setting in AIS328DQ

Posted on November 14, 2013 at 08:34Hi, The accelerometer was generating the interrupt when the value of CTRL REG 3 was  set to 0x80. But AS CHANGED TO 0x84 to check the latch interrupt request there is no more interruppt generation. Can anyone prov...

rehanar by Associate
  • 1001 Views
  • 1 replies
  • 0 kudos

L3GD20 data stability?

Posted on November 05, 2013 at 18:21Okay - I've got data flowing from the L3GD20 into the microcontroller using the DRDY/INT2 signal.  As I examine the readings that I am receiving from the sensor chip, though, it appears that I receive ''bogus'' va...

rich by Associate II
  • 1213 Views
  • 1 replies
  • 0 kudos

driver steval MKI062V2 for Win8

Posted on October 23, 2013 at 20:58Is it possible to download a driver for the steval MKI062V2 Inemo board in order to use it with windows 8?

caron by Associate
  • 1019 Views
  • 1 replies
  • 0 kudos

lsm9ds0 i2c interface

Posted on October 25, 2013 at 02:32I am getting data from the gyro from i2c address 0xd6 but I can't seem to get any response from the accelerometer at i2c address 0x3a.  Can anyone share any i2c code that works with accelerometer on this chip? #...

clovett by Associate
  • 744 Views
  • 0 replies
  • 0 kudos

L3GD20 DRDY signal issues

Posted on October 21, 2013 at 14:34Hello.  I want to process each set of readings from the L3GD20 as they become available.  The DRDY signal seems the most appropriate way to do this.  I've verified with an STMicro engineer that my register settings...

rich by Associate II
  • 1322 Views
  • 2 replies
  • 0 kudos