how to get accelerometer continuous data
Posted on May 29, 2014 at 15:15The original post was too long to process during our migration. Please click on the attachment to read the original post.
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Posted on May 29, 2014 at 15:15The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on May 29, 2014 at 12:33Hi guys/gals,I am new to the iNemo board and to ARM programming in general.I have just bought the iNemo-M1 discovery board, the STM32 programmer by ST, downloaded the firmware and installed the drivers. I have also ins...
Posted on May 28, 2014 at 15:01ST parts with an I2C interface use a restart in a multibyte read transfer. Instead of a restart, does the more conventional stop, start sequence work with the I2C interface in ST parts? Image is attached.
Posted on May 28, 2014 at 02:57Hi: I want to enable motion interrupt for accelerometer, but In LSM9DS0 datasheet, there's no description about Duration and Threshold register, Could you give me the example about how to set these two register to en...
Posted on May 26, 2014 at 09:13What is the FlightSense trademark, associated to VL6180X ? #vl6180x #flightsense
Posted on February 27, 2014 at 16:52Hi,My raw readings from the accelerometer of the LSM9DS0 MEMS have a big offset in two axis, it's about 0.15 G in the x-axis and .07 G in the z-axis. i find these offsets about 15% and 7% in these axis are a bit ...
Posted on October 30, 2013 at 12:48Dear all,I am working on the LIS3DH and trying to correctly develop the embedded Self Test feature.All I do is evaluating the difference between the ''Normal Measurements'' and the ''Self Test Measurements'' and ch...
Posted on May 19, 2014 at 09:17I try use LIS331EB in IAR 7.1 in one big project. Where can I find all additional files for IAR (startup_lis331eb.s, StdPeriph_Driver, StdPeriph_Examples )? Should I use core_cm0.h or You can give me something like l...
Posted on May 16, 2014 at 13:36Hello, I have some problems to understand the table 21(page31 in datasheet). The output rate is clear, but what does the bandwith means? Witch unit have the cut-off term and how did it have influence to my output value...
Posted on May 13, 2014 at 20:25The original post was too long to process during our migration. Please click on the attachment to read the original post.