MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Working with L3GD20

Posted on October 05, 2016 at 10:46I want to use my STM32F429 Discovery's on board L3GD20 to measure an angle from the horizontal, so I only need one axis. I am able to read the acceleration data but I am unsure about a few things: 1. What do I do w...

LSM9DS0 Sensor not giving Acknowledgement

Posted on August 19, 2016 at 06:37Hello, We are working on 9 Axis Sensor : LSM9DS0 which is interfaced with MCU over I2C interface. Please find the attached circuit diagram for your reference. Also, We have checked using evaluation board (STEVAL-MKI...

bhavin by Associate II
  • 1438 Views
  • 1 replies
  • 0 kudos

LPS22HB Attach process Flux

Posted on November 16, 2016 at 17:25Which flux is best for attachment of this product?  Is this device susceptible to damage if cleaned using an aqueous wash?

stst9182 by Associate
  • 723 Views
  • 0 replies
  • 0 kudos

LIS3DH high-pass filter not working

Posted on March 16, 2015 at 07:14At work I am using the LIS3DH accelerometer to detect body motion.  It is configured for +/-2 gs, 50 samples per second, with Streaming FIFO.  The watermark works fine for determining when the FIFO needs to be emptie...

microbob by Associate
  • 1613 Views
  • 2 replies
  • 0 kudos

Can be use accelerometer for Vibration measurement?

Posted on November 09, 2016 at 07:32I am using LIS332AR mems chip for vibration measurement. Assembled this chip in PCB and PCB located vertical with respect to ground. For every 90 degree rotation of this chip corresponding X and Y axis value chang...

LISDH12 high consumption

Posted on November 03, 2016 at 17:34Hi all,i use an accelerometer  LISDH12, and it have a very high consumption (400 uA).I have this configuration; SCL/SDA connect to vdd with 4.7kCS to high because i want to use a i2cSDA0 put on groundSomeone hav...

anna by Associate
  • 1003 Views
  • 3 replies
  • 0 kudos