MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM9DS1 Android Stack

Posted on June 21, 2017 at 10:25Hi, I am using LSM9DS1 IMU for one of our android-6.0 based product. As referred in below links,HAL Layer :  https://github.com/STMicroelectronics/STMems_Android_Sensor_HAL_Input Drivers:https://github.com/STMicroelec...

Gesture recognition with SensorTile

Posted on June 19, 2017 at 17:41Hi at all,I am trying to implement gesture recognition with a SensorTile, to develope my firmware I started studying the BlueMicrosystem2 example, and so I was able to detect simple gestures as the wrist's orientation...

lsm6ds3

Posted on December 12, 2016 at 14:48We need Linux device drivers of lsm6ds3 for kernel 3.7.6.Can somebody provide drivers

Does ST have plan to make SPI version of VL53L0x?

Posted on January 20, 2017 at 06:43I wonder that ST has plan to make another enhanced version of VL53L0x.VL53L0x's I2C speed and output rate is slow.If a spi interfaced device is made, I hope that it would support the daisy chain.Currently multiple ...

just4you by Associate III
  • 1073 Views
  • 1 replies
  • 0 kudos

LIS3DH SPI pull-up values?

Posted on December 19, 2013 at 17:28In LIS3DH datasheet (Doc ID 17530) on figure 3 page 12/42 we can see: ''When no communication is on-going, data on CS, SPC, SDI and SDO are driven by internal pull-up resistors.'' What is the pull-up value? Are t...

Mich1 by Associate III
  • 1170 Views
  • 3 replies
  • 0 kudos

H3LIS200DL Readings and Conversion

Posted on June 13, 2017 at 06:03Hello:I am getting some bizarre values from this device, and maybe it's not configured correctly, or I am not reading it correctly.It appears I can send and read from the device. I can use the 'WHO_AM_I' and get back ...

LSM9DS1 Gyroscope does not work?

Posted on June 08, 2017 at 16:57Hi all,I am testing a LSM9DS1 module to replace a L3GD20. I get readouts for the gyro, the accellerometer and the magnetometer. However when I turn my pcb I can see value changes on the accellerometer and the magnetom...

0690X00000603rqQAA.jpg

lis3mdl vs lsm9ds0

Posted on June 12, 2017 at 20:42Hi,Some time ago I've succesfuly used lsm9ds0 (SparkFun) for 3D magnetic field readings. Today I'm trying to upgrade my device to use lis3mdl (MinIMU-9 v5 Gyro) but the magnetometer output is different than lsm and I ...