MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS12DH12TR self test values

Posted on December 18, 2017 at 15:26Hi,  I am using LIS2DH12TR accelerometer. I am testing self test values.When self test mode is disabled, the axis values:Ax:100By:80Cz:90When self test mode is enabled in self test mode 1, the axis values:Kx:120Ly...

BlueNRG-MS

Posted on December 20, 2017 at 09:44Hello,I am working with the SPBTLE-RF module interfaced with a freescale IMX6 microcontroller.Right now I am porting the Beacon example code to my platform (WEC2013) and I am facing an issue with the SPI communica...

LSM6DS3 FIFO

Posted on December 19, 2017 at 13:40Hello,i am trying to use the FIFO of the LSM6DS3 unit and i have the following problem. I only buffer accelerometer's data so when i set the ODR for the accelerometer over 56Hz, (104, 208, 416, 833Hz etc), the buf...

Alex Dim by Associate II
  • 892 Views
  • 0 replies
  • 0 kudos

Low power accelerometer with shake detection

Posted on November 19, 2017 at 02:58Hello,Is there any low power compact accelerometer available from ST that can or configured to auto detect a shake like iPhone 'undo/redo shake' and interrupt host MCU to wake up. I don't want process acceleromete...

LSM303AGR

Posted on December 13, 2017 at 12:24 Hi, I have a question about the LSM303AGR. Now, we are using the LSM303D but it will be obsolete. So we are thinking to use the LSM303AGR which is equivalent. We saw an issue with the LSM303D about the po...

Vibration measurement sensors

Posted on August 11, 2017 at 10:20Dear,all:      ST companies have used for vibration measuring acceleration sensor? Requirements are as follows:Frequency response: more than 1khRange: 0-40 gPower:Low power consumptionUsed in water pump, fan...

Andy Zh by Associate II
  • 1563 Views
  • 3 replies
  • 0 kudos

Resolved! IIS2dh multi-byte read doesn't work?

Posted on December 05, 2017 at 23:07Hello ST Community,I have an application using the IIS2DH MEMS accelerometer. I was running into some issues, so to troubleshoot, I bought the STEVAL-MKI168V1 daughter board and SEVAL-MKI109V2 mother board. Using ...

Jeff Gros by Associate III
  • 2293 Views
  • 5 replies
  • 0 kudos

LIS2DH not driving INT2 pin

Posted on December 05, 2017 at 13:15hi,I'm trying to program a LIS2DH via I2C, with a stm32l151rb. I'm interested in the activity mode, in order to wake up the stm32l1 using the INT2 pin connected to one micro's wake-up pin.my configuration is:/*CTR...