MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Continuously varying output from MEMS Gyroscope

We are using the X-STM32MP-GNSS2 (with the STM32 discovery board DK2), which has ISM330DHCX IMU. The accelerometer readings seem fine from the IMU, but the gyroscope gives enormously high and varying readings even when we are stationary. See below th...

STEVAL-PROTEUS: Serial Monitor over Micro USB

Hi all!I've recently started working on a fault classification model utilizing the proteus1 board and the NEAI studio suite. I'd ideally like to set up a serial datalogger via the onboard micro USB to both obtain and display readings, alongside bench...

Haze by Associate II
  • 1961 Views
  • 2 replies
  • 0 kudos

Resolved! ST notifies termination of the following product: LIS3MDLTR

We embed LIS3MDLTR on our board that we produce, because this has high sensitivity: 6842 LSB/gauss. This corresponds to 0.146 mgauss/LSB, if I convert correctly. The other products has significanltly lower sensitivity: 1.5 mgauss/LSB. What are you pr...

tcseh by Associate
  • 5439 Views
  • 11 replies
  • 5 kudos

LPS22HBTR and PCB cleaning

Dear ST/Forum,We are using the LPS22HBTR pressure-temperature sensor in some PCB assemblies.Due to some cleanliness requirements of the experiment, I need to be able to clean the PCB this device is attached to but due to the very fine holes in the li...

DuncanR by Associate II
  • 3142 Views
  • 4 replies
  • 0 kudos

Resolved! ST1VAFE3BX basic MEMS Studio not behaving as expected

Are there any plans to have a video tutorial on the biosensor eval board?  (ST1VAFE3BX)? I connected it to MEMS Studio via the MKI109V3.  I'm experimenting with the "Features Demo" but it's not behaving as I expect.  Perhaps there's documentation abo...

Rauscher by Associate II
  • 1923 Views
  • 5 replies
  • 2 kudos

Resolved! Mems studio fsm debug

I am using Mems-Studio for my FSM project. I am testing the state machine, and everything is working fine; I can see interrupts. However, in the debug tab, when debug mode is enabled, the table does not compile, and I cannot observe the program's beh...

SamuPre_0-1738754405575.png
SamuPre by Associate II
  • 1755 Views
  • 1 replies
  • 0 kudos

LPS22HBTR pressure range query

Dear ST/Forum,Preamble:We are using the LPS22HBTR pressure-temperature sensor in some PCB assemblies.The data sheet indicates a pressure reading range with defined accuracy from 260 to 1260hPA/millibar and an absolute maximum overpressure value of 2M...

DuncanR by Associate II
  • 828 Views
  • 0 replies
  • 0 kudos

ILPS22QS: SWRESET bit not clearing

We are currently trying to run experiments with the ILPS22QS sensor. According to the datasheet, when setting the SWRESET bit in the CTRL2 register to 1, it should self-clear when the reset is finished - but this never happens. The bit stays 1, and t...