MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL6180 Eye Safety

Posted on May 22, 2018 at 00:36Ok, I know that ST's standard answer is that the VCSEL in the VL6180 is eye safe, and I have not problem believing it.  But when getting my product certified eye safe, the testing house does not just take our word for ...

How to improve ToF VL6180x field of view

Posted on May 22, 2018 at 04:09i recently conduct a scanning process using ToF sensor. I put a object which i expects 90 degrees square wave as output. But i eventually got a curve slope that is totally different from what i expect. Kindly advise on...

0690X0000060BCxQAM.png
Isaac Ng by Associate
  • 792 Views
  • 0 replies
  • 0 kudos

LSM 330 interrupt

Posted on May 21, 2018 at 11:02I am using LSM330 but not getting accelerometer and gyroscope interrupt when it exceeds threshold value. Gyrsocsope and accelerometer value changes continously even if the device is in stationary state. DEN_G is not us...

LSM6DS3 implementation

Posted on December 07, 2017 at 07:11Hi, I'm using the LSM6DS3 inertial module to implement 6D orientation detection, single tap & activity/inactivity detection.I also need the module to go into sleep mode when no activity occurs.Can you share the im...

How to enable Left/Right VL53L1X ranging sensor?

Posted on March 22, 2018 at 03:37Description:We encounter one problem when we port VL53L1X ranging sensors (left/center/right) to our platform STM32F429 controller, the left/right sensors can not be activated via I2C slave address 0x54 and 0x58. (ce...

leo su by Associate II
  • 1218 Views
  • 2 replies
  • 0 kudos

VL53L1X Multizone Scanning

Posted on May 17, 2018 at 16:54Hello guys,has anyone successfully used the multi ROI scan of the VL53L1X  camera yet? I'm still trying to get it to work but the reportings are not clear to me (can't just trigger one corner to report smaller distance...

VL6180X increasing the Range

Posted on May 04, 2016 at 11:37Hi, i would like to increase the range of the VL6180X but i don't know which register i have to modify. I see the code in the RangingAndALS_NucleoXXX sample but i don't understand how the VL6180X register have been mod...

About LSM6D33

Posted on May 16, 2018 at 21:20Hi, what is the bandwidth of the gyroscopes analog anti-aliasing filter?

Temperature sensor on ISM330DLC

Posted on May 14, 2018 at 16:11Hello, can you please tell if the temperature sensor on ISM330DLC returns absolute temperature values or the difference values with respect to a reference? Just read a thread (https://community.st.com/0D50X00009XkXfjSA...

NUCLEO-F207ZG - X-NUCLEO-CCA02M1 sound acquire

Posted on May 16, 2018 at 15:55Hello, i`m trying to get data from X-NUCLEO-CCA02M1 to my NUCLEO-F207ZG  vis I2s2 and i2s3, but unfortunetly i have even no I2SX_SCK on my device, what can be wrong ? I set transmission mode  to mode master recieve.Tha...

0690X0000060KnUQAU.png