MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lmsdso32 spi fifo reading using rounding issue

To make a successful read via the spi bus of the fifo in rouding mode should return 7 bytes, the tag byte plus 3 words but the device does not return correct data or count as a successful fifo (and update the fifo size). What data is returned is rubb...

MByrn.2 by Associate
  • 847 Views
  • 0 replies
  • 0 kudos

lmsdso32 fifo read rounding does not operate according to the data sheet application notes as it did for us the lms6dsl. Any ideas on why not would be appreciated

to make a successful read via the spi bus of the fifo in rouding mode should return 7 bytes, the 3 tag byte plus 3 words does not return correct data or count as a successful fifo (and update the fifo size). What data is returned is rubbish data. we...

MByrn.2 by Associate
  • 896 Views
  • 0 replies
  • 0 kudos

Use BDU on LSM6DS3(3) FIFO registers?

The LSM6DS3's datasheet recommends setting BDU=0 for the FIFO's status and data registers, which makes sense in my opinion.The LSM6DS33's datasheet recommends setting BDU=1 for the same register block, however. I can't find any recommendations for s...

Resolved! Is it possible to measure sound intensity level from PCM samples?

I am using two PDM microphones(mems transducer) with STM32 to measure the intensity and if the intensity of the left microphone is higher than the right one then an LED should turn on and vice versa.We measure the intensity of analog signals like whe...

Viki by Associate II
  • 6233 Views
  • 4 replies
  • 0 kudos

STEVAL-PROTEUS1

1) Please tell me how to mount the micro SD on the STEVAL-PROTEUS1.2) Please tell me how to test the above parts in the Windows10 environment as in the Android environment (st ble sensor).

BLee.9 by Associate
  • 711 Views
  • 0 replies
  • 0 kudos

Doubts about the reconfiguration procedure of the LIS2DUXS12's FSM

Hi support,I'm using the LIS2DUXS12. I make you a short recap about the use of the LIS2DUXS12 with our prototype:We use 3 FSM:FSM_1: To detect the significant motion;FSM_2: To detetct the no motion;FSM_3: To detect the situation where the acceleratio...

GPomp.1 by Associate III
  • 2367 Views
  • 5 replies
  • 0 kudos

Incorrect LSM303AGR Accelerometer Data

I'm trying to interface with the LSM303AGR using the 3-wire SPI protocol. I'm polling the registers 0x28 - 0x2D in high-accuracy mode, and what I've noticed is that the least-significant nibble of each axis is occasionally 0x1 instead of 0x0 as expec...

ESun.1 by Associate
  • 1680 Views
  • 2 replies
  • 0 kudos