G474 How to enable FDCAN error callback?
G474 How to enable FDCAN error callback?
G474 How to enable FDCAN error callback?
Hi all, I am trying to run a program from STM32cubeIDE to my STEVAL-MKI109V3 board, however the IDE is not recognizing my board. The device is listed in Device Manager under Ports&COMs as "STMicroelectronics Virtual COM Port (COM5)" so this leads me ...
While I was running STM32CubeIDE 1.14.0 today I was notified that there were updates available. So I clicked on the alert note and got suggested to update ST32CubeIDE and it ran into an error: An error occurred while collecting items to be installed ...
hello.I am creating a new development environment with this new PC purchase.I installed the latest version(1.14.0) of CubeIDE and imported the old project that was building normally. I expect it to build fine, but you get an error while building the ...
Is there any way we can actually stop the Cube from deleting pin names just because we change the pin function?I had hoped that "pin locking" would do it but no, if I spent ages naming all the signals on my MCU to line up with my hardware and then re...
Hi STI generally appreciate your tools and how to keep on make them better, keeping also quality on track.But let me say this: It is highly annoying that it is mandatory to login in the CubeMX and CubeIDE.Please remove this again.Use case: as a embed...
In following up with excellent tutorial for GPDMA between ADC12 and USART1 (removed 2D address) via this linkhttps://rristm.github.io/tomas_materials_v2/RRISTM/stm32u5_workshop/master/6_gpdma_handson_events_intro.md/Based on the event and ioc file fr...
The following project is imported in the latest Cube IDE (see below for version info) in an empty, new created workspace: When the IOC file is opened / code is generated, the following pop up appears (this is also the case when importing the example...
i tried to build a simple audio player , data from SD-card to USB audio host.audio host is a big mystery , only (in STM world) one (!) example now, with Azure rtos + USBx .(CubeIDE 1.13.1 , H563zit-nucleo board )ok, seem to work now, but SD-card read...
Hello,I'm using STM32F410 for ADC in which i have configured two channels means two conversions.For IN7 channel the input voltage is 1.89V and for IN8 input voltage is 2.0v(This channel we have connected trimpot voltage can varied ) Please check the...