STM32 MCUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I cant able to load the code Because Over Current (RED) LED is glowing on my STM32H743 Micro Controller . What is the cause and What is the solution for it so that i can load the code again ?

Hello,Iam using STM32H743 Nucleo board.Suddenly The Red LED (Over current LED) is glowing in my Micro controller. I have cheked all the connections properly there is no short circuit in it. Because of this i cant able to load the Program in it It is ...

MGane by Associate II
  • 1174 Views
  • 2 replies
  • 0 kudos

Can ST-link V2 programmer Connected to STM32H750VBT6 With 3Pin(SWDIO&SWCLK&GND) and Program it with keiluVisionV5.24a ???

Hello friends.I want to program my software to STM32H750VBT6.i Have a st-link v2 usb programmer with SWDIO pin , SWCLK pin ,RST,SWIM and 3.3V & 5V&GND on it,i connected SWDIO ,SWCLK and GND pins to My MicroController.in Debug Of Keil ( Option and tar...

MFarh by Associate II
  • 413 Views
  • 4 replies
  • 0 kudos