User Activity

LCDHi all. I can’t figure out how to work in LCD interface mode. I check it with an analyzer and see that when writing a byte, instead of one FMC_NWE pulse, several are generated.
When using the delay function, I encountered an incomprehensible manifestation, for verification I brought a signal to the output of the microcontroller and received a switching frequency two times lower. I checked SystemCoreClock, it shows the confi...
Good day. Faced such a problem. I wrote a loader for a non standard board, using stm32f476vgt MK, N25Q128A memory in extended SPI mode. All functions are tested in debugger mode. The data is written correctly, the memory is erased correctly, but veri...
Microcontroller stm32f030f4p6 is defined but not flashed in CubeIDE 1.11.0. It gives the message "The microcontroller is not original", while the CubeProgrammer flashes it perfectly, correctly determines the ID 0x444 Rev 1.0. If I try to flash it, it...
when trying to write the firmware to the flash of the controller, an error is displayed that the program cannot connect to the flash. At the same time, the CubeProg controller sees, reads, flashes. In Keil ver. 25, everything is fine, in older versio...
Kudos from