STM32 MCUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST-LINK V2 COM Port

Hi, I have an issue with CubeIDE and ST-LINK.I'm trying USART communication with STM32F0F4, I write code and debug but I don't get COM Port. In device manager there is no port showing. I installed st-link009.In CubeIDE, i tried both St-Link GDB Serve...

0693W00000Su1Q4QAJ.png 0693W00000Su1QJQAZ.png
lre.1 by Associate II
  • 1011 Views
  • 4 replies
  • 2 kudos

Resolved! NUCLEO-H503RB Debugging Issues

So as these things go I have an, two actually, ST NUCLEO-H503RB dev board that I cannot get the debugger to work with it.  My colleague on the other side of the country has the same boards and a similar setup and he is having no problems debugging.  ...

JChrist_0-1717969403672.png
J.Christ by Associate II
  • 351 Views
  • 5 replies
  • 2 kudos

Resolved! STM32GO controller PWM Generation issue

Hello AllCurrent Device setup:-NUCLEO-G071RB Eval boardSTM32CubeMX settings please find the attached screenshots.I'm trying to generate PWM signal using [ TIM3 channel 3] in NUCLEO-G071RB Eval board.Time period is 28 microseconds and width are 3 micr...

Denial1_0-1697024584663.png Denial1_1-1697024584665.png
Denial1 by Associate II
  • 1435 Views
  • 10 replies
  • 2 kudos

SWO Viewer in ST-LINK Utility

Hi Friends, I need Yours Help. I have  working on  STM32F407VET6  development board  and  I have to write on simple code like count the values. I want to see the data in SWO (Serial Wire Viewer).But using STM32CUBEIDE to flash the code to my code is ...

Vignesh_V by Associate II
  • 1577 Views
  • 22 replies
  • 3 kudos