2023-10-11 4:45 AM
Solved! Go to Solution.
2024-06-06 4:54 AM
Hello @waclawek.jan, @Denial1, @TDK,
This behavior is now noted in Readme files of all HAL TIM examples calling HAL_TIM_PWM_ConfigChannel() with the output channel configured in PWM1 mode:
TIM_6Steps,
TIM_Asymetric,
TIM_CascadeSynchro,
TIM_Combined,
TIM_ComplementarySignals,
TIM_Dithering,
TIM_DMA,
TIM_DMABurst,
TIM_ParallelSynchro,
TIM_PrescalerSelection,
TIM_PWMOutput.
The note is the following:
In this examples, the output channel is configured in PWM1 mode meaning that in up-counting mode, channel 1 is active as long as TIMx_CNT < TIMx_CCR1. As, in the function HAL_TIM_PWM_Start* function, the output channel is enabled prior enabling the timer's counter a timing difference might be observed on the first generated PWM. This difference corresponds to the delay - in term of number of CPU cycles - between the channel enable and the counter enable in the HAL_TIM_PWM_Start* function.
Thank you!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-11 6:43 AM
Hello @Denial1,
Are you overwriting the CCR register directly? Have you seen this behavior after changing the pulse width from 7us to 3us?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-11 6:47 AM
Probably the first pulse starts before the timer is started.
A solution would be to set the CNT of the timer to a value which produces a low state on the pin, rather than a high state. Perhaps set to ARR-1 instead of 0 during initialization. Or otherwise ensure the output state is low during initialization.
2023-10-13 2:02 AM
Hi @Sarra.S
I'm using HAL library function to start the PWM
HAL_TIM_PWM_Start_IT(&htim3); and
HAL_TIM_PWM_Stop_IT(&htim3) to stop the PWM.
2023-10-13 2:06 AM
Hi @TDK
I have attached screenshots of STM32cubemx settings. Please look into this.
2023-10-16 2:06 AM
Hello again @Denial1,
I am afraid I couldn't reproduce the issue using the example of the STM32Cube_FW_G0_V1.6.0 package.
So, could you please specify the sequence to reproduce it; have you changed the PSC register value? I am thinking that during the first timer period timer works with another PSC from previous configuration
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-18 12:22 AM
Hi @Sarra.S
Thanks for your response!!!!
Path for the example code: -
STM32Cube_FW_G0_V1.6.0\Projects\NUCLEO-G071RB\Examples\TIM\TIM_PWMOutput
I have not changed anything in this example code.
The output can be observed, as shown in the below image 1.
Pin No PA8, PA9, PA10 and PA11 all are having corrupted/ different pulse width of first pulse.
You can easily reproduce this issue, without making any changes to example code.
Looking for your reply!!
Regards,
Denial
2023-10-18 2:01 AM
Hello again @Denial1,
Actually, that's exactly what I did, using the same example with the same FW version with NUCLEO-G071RB.
As you can see, there is no first corrupted pulse.
PS: you mentioned "NUCLEO-G071RB Eval board", is that a typo or are you using a custom board?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-18 7:42 AM - edited 2023-10-18 7:43 AM
From the waveform capture it's not clear whether the leftmost pulse was the first one after reset (and I am afraid it wasn't).
CubeMX with Cube/HAL provides a quick clicking solution to generate PWM but perhaps does not pay much attention to details like this. If you want anything outside of what the Cube/HAL authors deem usual usage, Cube gets into way more than helps. TDK gave you above the explanation for your problem and also a suggested remedy, just follow his recommendation.
JW
2023-10-19 6:00 AM
@Denial1 I apologize for the previous mistake. You're right @waclawek.jan!
I am tracking this issue with an internal ticket (Ticket 164283), I will keep you informed!
Sorry for the inconvenience.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.