Skip to main content
Associate II
June 2, 2024
Question

ST-LINK, ST-LINK/V2, ST-LINK/V2-1, STLINK-V3 USB driver signed for Windows7, Windows8, Windows10

  • June 2, 2024
  • 2 replies
  • 2865 views

Downloaded the subject driver and installed it per the instructions in the readme.txt (ran the batch file as admin)

"Device Driver Installation Wizard" dialog reports that the drivers (Qty 3) were successfully installed and ready to use.

Brian12412_0-1717305761518.png

In Windows "Device Manger" > "Other devices" the only entry is a pre-existing one "Bluetooth Peripheral Device"

What do I need to do to get the driver to show up in Device Manager?

Connected the board to the Windows computer using a USB to USB micro cable.

The ST-LINK LED flashes on/off about once per second.

This topic has been closed for replies.

2 replies

AScha.3
Super User
June 2, 2024

>What do I need to do to get the driver to show up in Device Manager?

Connect your st-link to usb->PC , then you see : in Device Manager - or not. :)

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
June 2, 2024

Nothing changes when STM32L475 is connected to the PC via USB.  Still nothing in Device Manager.

AScha.3
Super User
June 3, 2024

>Nothing changes when STM32L475 is connected to the PC via USB

WHAT you connect then ?  nucleo or custom board ? using st-link - or not ? or boot mode ?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
June 11, 2024

Factory STM32L475 connected to Windows 11 PC via USB cable.

AScha.3
Super User
June 11, 2024

>Factory STM32L475

Well, most chips coming from a factory...so show a pic, what you connect then really.

+

nucleo or custom board ? using st-link - or not ? or boot mode ?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
June 11, 2024

It is the "B-L475E-IOT01A Discovery kit".  ST-LINK is over USB.  The board (kit) is connected to a Windows 11 PC via USB cable.  The issue is with the drivers.