STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1383 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 546 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Validation on target falling on F4 Discovery

Hi, I'im running X-CUBE-AI with STM32Cube IDE on a F407 Discovery. When I try to perform validatation on target, I get the following error during building stage :  Building project /opt/st/stm32cubeide_1.18.1/plugins/com.st.stm32cube.ide.mcu.external...

PauloP by Associate
  • 689 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G4: trigger SPI DMA through GPIO EXTI event?

Hi, I want to get data from an ADC connected externally through SPI DMA whenever data ready pin is set. I want to do it without any interrupt handler, since our firmware have already loaded with other stuffs. I have tried the synchronisation of SPI D...

BrindhaP by Associate II
  • 4279 Views
  • 14 replies
  • 0 kudos

STM32N6 Index Problem

Hello,I am working on USB Device VCP project but I have problem about defines,index,etc. As you can see below that I have definition of "STM32N655xx" but I can not include "stm32n655xx.h".I tried Index, Rebuild step but it did not fix. On the other h...

BKaya_0-1750412741674.png BKaya_1-1750412775627.png BKaya_0-1750416360701.png
B.Kaya by Associate III
  • 980 Views
  • 2 replies
  • 0 kudos

Resolved! [Nucleo-N657X0-Q ]How to use swv printf in Keil arm mdk 5.39

I would like to use SWV for debugging on the Nucleo-N657X0-Q board.I first enabled SWV debugging and also change the CPU clock to 400 MHz.   Then, I added some code to main.c (as reference here ).At the same time, I also set the core clock to 50 MHz ...

image.png bioak_0-1750155820298.png bioak_3-1750157556553.png bioak_1-1750156771078.png
bioak by Associate II
  • 1241 Views
  • 2 replies
  • 2 kudos

cube ide strange breakpoint behaviour

Using cube IDE to debug my application i've witnessed breakpoints behaving unpredictably: sometimes they appear on their own in breakpoint list view while not present in the file editing view; other times the breakpoints i've just placed and just use...