User Activity

Hello, I just imported a shared project from DevOps and I had to change some absolute paths to project relative paths in Project Properties-C/C++ General-Paths and Symbols-Includes.Now I am still facing some errors like: "...No such file or directory...
Hello, I am building my own driver for ST25 device. After configuring the GPO I would like to read the register to make sure the config is applied. As said in datasheet I have to use this function:Which HAL function should I use ? I tried with these ...
Hello community, I am using STWINKT1B board and trying to implement basic accelerometer datalogging from scratch. I don't want to use HSDatalog because I don't need so many functionnalities.I am using FATFS functions, able to use mount, mkfs, mkdir, ...
Hello, I have as project to use the STWINKT1B board and write my custom code to read IMP23ABSU sensor at its maximum capacity (80kHz). I understand the sensor output data is amplified by an op-amp and can be read with ADC input of the microcontroller...
Hello everyone, I just have seen information from Azure about TLS Certificate critical changes : https://techcommunity.microsoft.com/t5/internet-of-things-blog/azure-iot-tls-critical-changes-are-almost-here-and-why-you/ba-p/2393169I am using x-cube-c...
Kudos given to