STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1467 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 570 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Flash memory & SD Card

Hello everyone, just I want to know a little detail: when I’m debugging my program (C file) I suppose it goes to the flash memory! I want to know if it’s possible to debug to SD Card?

idrissmc by Associate III
  • 1508 Views
  • 3 replies
  • 0 kudos

Follow others custom usb hid demo but not work.

I first used a stm32f103 board,after generated code and configurated usbd_custom_hid_if.c and then download the code,my computer cant recognize the usb device.Then I changed to a f407 board, after done the same work,my computer can recognize the devi...

Mcfly by Associate
  • 809 Views
  • 0 replies
  • 0 kudos

Repeatition counter problem in STM32G431RB DISCO + CubeIDE

Hello.There are some problems with the repeatition counter (TIMX_RCR).The problem occurs when I enable the OPM setting to use the feature and enter a 16 bit value in the RepetitionCounter setting.I think that it is correct to change uint8_t Repetitio...

MKim.5 by Associate
  • 1822 Views
  • 3 replies
  • 0 kudos

How to use GCov in STM32Cube IDE and STM32F4

Hello,I have tried to set up GCov in STM32Cube IDE using this tuto:https://mcuoneclipse.com/2014/12/26/code-coverage-for-embedded-target-with-eclipse-gcc-and-gcov/I am using a STM32F413 and when I compile I got an overflow on RAM section by 150Kbytes...

ABern by Associate II
  • 2527 Views
  • 0 replies
  • 4 kudos

printf float STM32G070CB

How to enable float (printf) in STM32CUBEIDE 1.0.1 IDE?The -u printf_float option is selected.

RDos by Associate II
  • 1509 Views
  • 2 replies
  • 0 kudos

Why do I get error when I build project?

Hello,Why do I get error when I build project?I have imported the projectCan anyone help me if I send the project files?With Kind regards / Peter16:12:11 **** Build of configuration Debug for project test ****make all C:\Program: C:\Program: Permissi...

0690X000009YD3CQAW.png
PStur by Associate
  • 1570 Views
  • 2 replies
  • 0 kudos

Resolved! Problem creating new C project

HiI am evaluating the new STM32CubeIDE .When trying to create a new project (based on an existing project done using eclipse + GNU ARM Eclipse) i am encountering a problem when accessing the project properties to define include directories; Preproces...