cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to load/debug STM32L432 Nucleo-32 on MAC OSX either on stlink-GDB or openPCD

RKatz
Associate II

Hi,

(running Mac OS Mojave 10.14.5)

I can not debug my program, on stlink- gdb I get the following console message:

STMicroelectronics ST-LINK GDB server. Version 5.2.3

Copyright (c) 2019, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    LogFile Name       : /Users/rankatz/STM32CubeIDE/workspace_1.0.1/Audio detector/Debug/st-link_gdbserver_log.txt

    Logging Level       : 31

    Listen Port Number    : 61234

    Status Refresh Delay   : 15s

    Verbose Mode       : Enabled

    SWD Debug         : Enabled

Hardware watchpoint supported by the target 

SWD frequency = 4000 kHz

ST-LINK Firmware version : V2J34S25

Device ID: 0x435

PC: 0x8004420

ST-LINK device status: HALT_MODE

ST-LINK detects target voltage = 3.26 V

ST-LINK device status: HALT_MODE

ST-LINK device initialization OK

Waiting for debugger connection...

Waiting for connection on port 61234...

Accepted connection on port 61234...

Debugger connected

Debugger connection lost.

Shutting down...

(log file is attached)

and when trying open OCD I get:

Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-06-12-13:24)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

srst_only separate srst_nogate srst_open_drain connect_assert_srst

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

padded zone erase set to 1

adapter speed: 8000 kHz

adapter_nsrst_delay: 100

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : clock speed 8000 kHz

Info : STLINK v2.1 JTAG v34 API v2 M25 VID 0x0483 PID 0x374B

Info : using stlink api v2

Info : Target voltage: 3.254557

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : Stlink adapter speed set to 4000 kHz

Info : STM32L432KCUx.cpu: hardware has 6 breakpoints, 4 watchpoints

Info : Listening on port 3333 for gdb connections

Info : accepting 'gdb' connection on tcp/3333

target halted due to debug-request, current mode: Thread 

xPSR: 0x01000000 pc: 0x08004420 msp: 0x200006d0

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : Stlink adapter speed set to 4000 kHz

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

adapter speed: 4000 kHz

Info : Device id = 0x10016435

Info : STM32L4xx flash size is 256kb, base address is 0x8000000

shutdown command invoked

Also tried re-installing the stlink server and the IDE - got the same results.

What am I doing wrong?

Thanks!

Ran

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
RKatz
Associate II

After searching some more onto web, found a workaround that worked for me: erased the flash contents (using the open source stlink's st-flash utility) .

After that I managed to load and debug several times (using st-link GDB server, did not try openOCD).

Hope this helps someone :)

View solution in original post

2 REPLIES 2
RKatz
Associate II

Attaching the GDB log file...

p.s. also tried re-installing the stlink server and the IDE - got the same results.

RKatz
Associate II

After searching some more onto web, found a workaround that worked for me: erased the flash contents (using the open source stlink's st-flash utility) .

After that I managed to load and debug several times (using st-link GDB server, did not try openOCD).

Hope this helps someone :)