User Activity

Hi list,I'm using stm32f103 and stm32cude ide. And I'm also using FreeRTOS.This is my stop mode code.This code is called in TimerCallback which is created from FreeRTOS.HAL_SuspendTick(); __HAL_RCC_PWR_CLK_ENABLE(); //HAL_PWR_EnterSTOPMode(PWR_MAINRE...
At first, I downloaded elf using stlink v2 and run firmware. and then rebuild source. After that I tried to run debug button. But I encountered no device message.
I am using ubuntu18.04. I've installed open jdk amd javagfx. But cube prog does not run due to javagfx.properties file. I searched under /usr directories. But I couldnt find out it at all.Could anyone help me?
When I installed at first CubeIDE, I could select FreeRTOS as middleware. But failed due to can't use systick as reference clock of FreeRTOS.After that, I can't choose a Middleware such as FreeRTOS, when I create New Project.What am I wrong?