Cube IDE 1.1 - debugger fails to connect under reset to erased H7 MCU
After full chip erase in Cube Programmer, the CubeIDE debugger cannot connect with any reset option : connect under reset or software system reset.
Says: "Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load xxxxx.elf.
Cube Programmer can connect to it with options:
- Under reset
- Core reset
Other options: hardware reset, software reset - both fail with "DEV_TARGET_NOT_HALTED"
Why Cube IDE debugger does not have this "Core reset" option? Can it be added, please?
The chip is STM32H750 with external ST-LINK/v2.
-- pa