STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1402 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Running STM32Cube IDE Debug on VMWare linux

Hi,I was curious if the community has had success and/or lack of it when running STM32 Cube IDE and reading the serial from Linux as a VMWare client, from a Windows host? Any issues bridging the USB connection through the Windows host, to the boar...

Sleepmode not working properly

Hello,I'm using a stm32f070f6 mcu.My problem is that, when I debug separately my bootloader and my APP code, everything works fine, but when I put them together in a hex file and upload it to my MCU(the bootloader remaps the IVT to the RAM before jum...

MCasas by Associate II
  • 1300 Views
  • 1 replies
  • 0 kudos

Resolved! Project copy/paste doesn't work

Hi all,Afer copy/paste of project cubemx .ioc file name is not updated accordingly and cannot be opened.Manual updating name of .ioc file is fixing this issue.Regards,Pawel

PHryn by Associate III
  • 2729 Views
  • 5 replies
  • 0 kudos

Resolved! CubeIDE flash problem

CubeIDE 1.0.2 deb linux.IDE see STlink.v2​, I sucessfully upgraded it.When I click on build (checked debug or release) project builds without errors but it dont flash target.​​Only once it flashed my board (disco f407vg) when messing with debug confi...

oeliks by Senior
  • 1066 Views
  • 2 replies
  • 0 kudos

BUG found! 'USBH_LS_SPEED' undeclared

When trying to compile a project with STM32F4 with USB FS Low Speed 1.5MBit / s this error occurs:../Drivers/STM32F4xx_HAL_Driver/Inc/stm32f4xx_hal_hcd.h:113:38: error: 'USBH_LS_SPEED' undeclared

by Not applicable
  • 1006 Views
  • 2 replies
  • 1 kudos

Hi, I've installed recently stm32cubeide. My questions are about navigating into project.. when i want to "find" something, the dialog box just find the "text" in the current header or c file, how can i change the setting to search in the whole project?

I also want to see where the defines or variables in the current page originate from?for functions its key "F3", but by variables and defines i don't know how to find them...

Fate1 by Associate II
  • 2918 Views
  • 6 replies
  • 0 kudos