STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1328 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 529 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Linking binary files for use in C++ application - how?

Hi there,I am new to the STM32 microcontrollers and the STM32 Cube IDE, and I'm tasked with including a binary set of data in a program. Most of the code is generated with the CubeMX program to help me with initialization. Please be advised, that I c...

NRoes.1 by Associate II
  • 4162 Views
  • 4 replies
  • 1 kudos

MAC Configuration STM32F4-Discovery board

I am using STM32CubeIDE to generate the code.The only MAC address that will work is 02:00:00:00:01. This address shows up inthe LWIP\Target\ethernetif.c file in the static (void low_level_init(struct netif *netif) function. If I change it to anything...

STM32H745ZI-Q - Debugging problem is STM32CubeIDE

I just have NUCLEO-STM32h745zi board. When I try to debug simple binking led aplication in STM32CubeIDE, this message appear: Break at address "0xa05f0000" with no debug information available, or outside of program code.I am using this application no...

KPiek by Associate
  • 1109 Views
  • 2 replies
  • 1 kudos

Resolved! Why can't I install Segger JLink Utilities?

There is a big issue I'm facing. I just installed STM32CubeIDE 1.2.0 but then I get an error when trying to install JLink_Linux_V662_x86_64.debI absolutely need those tools because I also do development for other boards with Segger JLink probes.What ...

0690X00000Bx9WXQAZ.png
m4l490n by Senior
  • 6320 Views
  • 4 replies
  • 1 kudos

how write c++ and include c++ lib in stm32CubeIDE?

hiin stm32CubeIDE c++ code and standard lib (#include <iostream> or #include <iostraem.h>) not work.i test:'convert C to C++'make c++ projectuse only c++ code in func main() ==> 'bool a = true;' all test not woke!!!ya khoda

kshin.111 by Associate III
  • 3081 Views
  • 3 replies
  • 0 kudos

[Solved] Infinite loop without "Warning: iteration N invokes undefined behavior", using pointers to get data from a function

I am citing this error here, just in case someone else has this type of occurrence.uint8_t data1[5];   for(uint8_t x = 0; x < 8; x++) { data1[x] = 0; }When using an array in a count loop above the limits of the array, the compiler can report a warni...

by Not applicable
  • 3961 Views
  • 0 replies
  • 0 kudos

Hi everyone Why the generated code is not stable?

I am using STM32cubeIDE and STM32f103ret6 chip on my board The schematic I used is here: https://github.com/mcauser/BLUE_BUTTON_F103RET6/blob/master/docs/STM32F103RET6_schematics.pdf​I have two problems the NRST after some time _between 5 minutes to ...

Mugtaba by Associate II
  • 3286 Views
  • 6 replies
  • 0 kudos