STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1369 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 539 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

code gets lost upon debug

I downloaded the STM32CubeF7 bundle and extracted it. Then made a new folder under the projects folder of the bundle and started STM32CubeIDE with the workspace pointing to the projects folder. I started a new project blinkled and put the blink code ...

KPort.1 by Associate
  • 1016 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeIDE Update not working

I get the following error during update in eclipse.An error occurred while collecting items to be installedsession context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).No repository found ...

BelSoft by Associate II
  • 9850 Views
  • 12 replies
  • 1 kudos

NUCLEO=STM32H745ZI-Q: problems with SPI1 and SPI3

Hello,I am new to STM32 dev, so...Logic analyzer only shows a glitch on MOSI line of SPI1 of around 156 ms then it puts it back to LOW level; similar results for SPI3.Using PB3 (D23) and PB5 (D22) for SPI3; using PA7 (D11) for SPI1; Solder bridges:...

kellogs by Associate II
  • 1317 Views
  • 2 replies
  • 0 kudos

Could anybody make Cubide work with STM32F7508-DK board?

first of all i had the FLASH problem (the MCU only has 64KB FLASH) so i brought up the external memory but is not possible to make debug aparently. As an evaluation board im a little dessapointed, couldnt find much support anywhere. i have been a cou...

martin.m by Associate
  • 655 Views
  • 0 replies
  • 0 kudos