STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1380 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 545 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Convert elf file into an srec file

I am using STM32CubeIDE, version 1.2.0. I want to convert the elf file into an srec file with a particular format. I have tried editing the command line in the Post-build steps to read:arm-none-eabi-objcopy.exe -O srec —srec-len=28 —srec-forceS3 “$(B...

erussell by Associate II
  • 5694 Views
  • 4 replies
  • 0 kudos

How can I add QSPI custom external loader to the debugger

In the Debug Configuration under the Debugger tab there is an option to add external QSPI loader .I have a custom external loader that is working with CubeProgrammer and STLinkUtility.I want to use this custom loader from within the CubeIDE.How can I...

Updating software has encounters a problem: I tried a few thing seen on eclipse sites but nothing works. Someone have an idea? Thanks.

An error occurred while collecting items to be installedsession context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).No repository found containing: osgi.bundle,org.eclipse.epp.mpc.core,1....

thecoach by Associate II
  • 2552 Views
  • 3 replies
  • 1 kudos

FPU

Probably a typo. In M4 generic user guide the mnemonic for floating-point MAC is shown as VLMA

ax0018 by Associate III
  • 1499 Views
  • 2 replies
  • 0 kudos

CMSIS FFT problem in stm32cubeIDE

I tried to compile and run arm_rfft_q15(STM32F030R8) .In STM32CubeIDE, I'm using libarm_cortexM0l_math.a, the file is in STM32Cube_FW_F0_V1.11.0\Drivers\CMSIS\Lib\GCC, one of the functions I'm using is arm_rfft_q15. Build error: undefined reference t...

LLily.1 by Associate II
  • 2817 Views
  • 4 replies
  • 0 kudos

Resolved! Can't connect to target after power off (STM32F769I-DISCO)

I have the STM32F769I-DISCO board and just made a simple application that uses usart1 to print some debug messages on the virtual com port (USART1. Everything works fine until I power off the board. When the board is connected to usb cable again the ...

0693W000000WSSgQAO.png
ALevc.1 by Associate III
  • 1434 Views
  • 2 replies
  • 0 kudos

STM32H750 + I2S Full Duplex Master + DMA (TX and RX)

Hello,I managed to get full duplex I2S + DMA working on an STM32F405 with Cube + HAL, however have now switched to an STM32H750 for more processing power.In STM32CubeIDE version 1.3.1, while there is an option to add a DMA stream for TX, there is unf...

PSalm.1 by Associate
  • 2394 Views
  • 2 replies
  • 0 kudos