STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1381 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 546 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Load external flash with STM32CubeIDE

I have a STM32CubeIDE project for STM32F769 board that has external flash (same as DISCO design). How do I configure the IDE so it will load both flash memories?

RWeil.1 by Associate II
  • 1114 Views
  • 1 replies
  • 1 kudos

How reconcile the address field within a SREC file?

Hi All,The STM32CubeIDE can produce a SREC file. I am trying to decode the Address field within the file.It should be 32 bit bigendian, however, it is 24 bit of an unknown endian style.Can someone please explain the endian style used?STM32CubeIDE Ver...

PSPF by Associate II
  • 1873 Views
  • 3 replies
  • 0 kudos

STM32CubeIDE breaks on macOS when upgrading from 1.3.0 to 1.3.1. The application cannot find java after upgrade. (Resolved)

The issue is an erroneous plist: /Applications/STM32CubeIDE.app/Contents/Info.plistThere are missing sections under the Eclipse key.Below is a functional Info.plist, please compare to yours and modify if need be...<?xml version="1.0" encoding="UTF-8"...

jan by Associate II
  • 762 Views
  • 0 replies
  • 1 kudos

Resolved! Custom linker won't compile

I'm trying to reserve space in RAM for emulated eeprom. I can read and write fine, however when I try to modify the linker it won't compile. The added user section/* Specify the memory areas */ MEMORY { FLASH (rx) : ORIGIN = 0x08000000, LENGT...

MBeau.1 by Associate
  • 2609 Views
  • 3 replies
  • 0 kudos