2020-05-26 11:02 AM
I'm trying to reserve space in RAM for emulated eeprom. I can read and write fine, however when I try to modify the linker it won't compile.
The added user section
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 96K
USER_DATA (rwx) : ORIGIN = ORIGIN(FLASH) + LENGTH(FLASH), LENGTH = 32K
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 8K
MEMORY_B1 (rx) : ORIGIN = 0x60000000, LENGTH = 0K
}Howerver when trying to compile it says «invalid character» at the line of the new section in the linker script:
c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe:../stm32_flash.ld:48: ignoring invalid character `\342' in expression
c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe:../stm32_flash.ld:48: ignoring invalid character `\200' in expression
attempt to open c:/st/stm32cubeide_1.3.0/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610/tools/bin/../lib/gcc/arm-none-eabi/7.3.1/thumb/v7-m\libm.a failed
c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe:../stm32_flash.ld:48: ignoring invalid character `\254' in expression
c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe:../stm32_flash.ld:48: ignoring invalid character `\342' in expression
c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe:../stm32_flash.ld:48: ignoring invalid character `\200' in expression
Solved! Go to Solution.
2020-05-26 6:35 PM
You have unicode characters in your script which should be strictly ASCII.
Delete the line it's complaining about and retype it on the keyboard. Don't copy/paste.
2020-05-26 6:35 PM
You have unicode characters in your script which should be strictly ASCII.
Delete the line it's complaining about and retype it on the keyboard. Don't copy/paste.
2020-05-27 6:40 AM
It did the trick, I used a different editor as well.
2020-05-27 7:51 AM
Pasting via generic Notepad app can strip formatting.