STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1409 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 557 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

SWV Exception Trace is not working in STM32CubeIDE

I want to trace exceptions/interrupts happening in my board with STM32L4xx in STM32CubeIDE by `SWV Exception Trace Log` and `SWV Trace Log`. I use SEGGER J-Link and In Debugger I have correctly set the interface to SWD and the Core Clock to 80 MHz. A...

KK.1 by Associate
  • 1059 Views
  • 0 replies
  • 1 kudos

unknown type name '_ARMABI'

Hi Sir,I'm transferring code from Keil to CubeIDE. During compilation, i cannot find the way to solve the error unknown type name '_ARMABI'. _ARMABI is defined in many header files including stdio.h and time.h in Keil environment, but I cannot find w...

LChan.5 by Associate II
  • 1114 Views
  • 1 replies
  • 0 kudos

Is there an example of smbus master and slave usage ?

I am trying to use smbus to talk to a charger chip. Is there any example on how this works ?I am using the following HAL API.HAL_SMBUS_Master_Receive_IT(&hsmbus1, 0x0b, &reg_val[0], sizeof(reg_val), SMBUS_FIRST_AND_LAST_FRAME_NO_PEC);IRQ handler:void...

PRedd.111 by Associate III
  • 1526 Views
  • 1 replies
  • 0 kudos

Can't make running the basic USB training

Hey guys! I am desperately trying to make a basic USB between my stm32 (stm32L073RZT6) and my linux working... I wanted to discover stm32 and it's STM32CubeIDE so i am new to this and i am doing the USB tutorial consisting only to send a message to a...

Jmaxi by Associate II
  • 1751 Views
  • 2 replies
  • 0 kudos

eclipse installation problem

Dear ST Hello,I want to use eclipse for my stm32f board.I installed the arm gnu tool chain and the package gnu from my eclipse installer.I added the \bin to my PATH in eclipse and OS.I couldn't compile the project, it seems like eclipse couldn't find...

0693W000001shlqQAA.png 0693W000001shllQAA.png

how to use st link and connect GDB server in cube Ide

 hi, I'm using STM32CubeIDE 1.3.1 and trying to execute some programs. but there's a this message. it seems the problem relay upgrading st link and GDB server but I don't know how to solve this. do anyone have the same problem? I'm using STM32CubeID...

0693W000001shWbQAI.png
T22 by Associate II
  • 2408 Views
  • 4 replies
  • 0 kudos