STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1439 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Why can't I communicate with the USB_OTG_FS interface in CDC anymore when I enable the I2C1 communication port in the STM32H743I_EVAL2 board?

Hello ST Team,I developped a USB OTG FS in CDC class, using advices from ST's tutorials in Youtube and I managed to send data received from the USB reception buffer to another one I want to use for I2C communication.However, when I enable the I2C1 an...

0693W000003Q10pQAC.png 0693W000003Q11EQAS.png 0693W000003Q12RQAS.png 0693W000003Q135QAC.png
BNord.1 by Associate III
  • 2180 Views
  • 3 replies
  • 0 kudos

STM32F405RG ADC problem

Hi I am trying to sample an external signal with the ADC inside STM32F405RG MCU.You can see the code below.#include "main.h" #include "SysClockConfiguration.h"   uint16_t ADC_Buffer0[1000]; uint16_t ADC_Buffer1[1000];   void Dummy_Delay(uint32_t x) {...

KHoca.1 by Associate
  • 1539 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeIDE Combine projects

STM32CubeIDE Support,How are projects combined when there are more than one project? I didn't figure out the methods.Best regards,Adam

AXu.11 by Associate III
  • 2227 Views
  • 3 replies
  • 0 kudos

Resolved! Any plan to upgrade STM32CubeIDE toolchain?

I've seen there are several posts with similar questions, but no real answer.I'm would like to know if there are plans to upgrade the GCC toolchain in the near future?Like many, I am interested in using C++17 features, so GCC 9 would be desirable.CC:...

Armandas by Associate III
  • 1529 Views
  • 2 replies
  • 1 kudos