STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1527 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 581 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Debugging Nucleo-F401RE with st-link

I am trying to debug a a nucleo-F401RE with the st-link. About a week ago, it was fine and the code uploaded. I had made it so that the LED on the F401RE turned on and off when I pushed down and released the push button. I came back to it yesterday t...

VZerb.1 by Associate II
  • 7040 Views
  • 11 replies
  • 0 kudos

[STM32F4] Multiple CAN filters using HAL

Good morning,I'm using a CAN bus on my STM32F446RE. Right, now, the CAN communication is working with only one rx filter. I saw in datasheet that we can use up to 128 filters. I don't need so many filters, but I'm trying to configure a second filter....

0693W000006ESbbQAG.png
ValentinG by Associate II
  • 1970 Views
  • 0 replies
  • 0 kudos

Battery management system with stm32F407G and Bare Metal Coding Hello, I would like to design Battery management system

I need just measuring current and voltage of 24 batteriesand accoring to datas, some actions should be taken(stop motor drive,starting of fans vsvsvs)I used,keil microvision,,ATOLLIC true studio, and also Cube IDEBut, I always have problems with libr...

SArsl.1 by Associate II
  • 3396 Views
  • 1 replies
  • 0 kudos

En el Stm32cubeide versión 1.3 existe alguna forma de crear algún proyecto escrito netamente en lenguaje ASM; uso la placa Discovery st.m32f429izt

En el Stm32cubeide versión 1.3 existe alguna forma de crear y escribir algún proyecto netamente en lenguaje ASM; uso la placa Discovery st.m32f429izt; lo que busco es un compilador netamente en ASM que trabaje en el CUBEIDE.Gracias.

LZamb.3 by Associate II
  • 2011 Views
  • 3 replies
  • 0 kudos

Resolved! Finding the function beeing interrupted

Hello,I used to work with IAR.In IAR call stack, if ever you break into an ISR, the call stack shows you where you were in the "main" code just before the ISR fired.Now, with STM32Cube MX, the call stack only shows the call stack since the root ISR ...

Kuikui by Associate III
  • 3160 Views
  • 4 replies
  • 1 kudos