STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1427 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

C++ Project on STM32CubeIDE

Hi,my name is Davide Urbano and I'm using STM32CubeIDE making only C projects; now I'd like to create a C++ project so going to File->New ->STM32 Project and selecting my stm32 mcu, I check for a C++ language project. The project created has only C f...

DUrbano by Associate III
  • 5055 Views
  • 8 replies
  • 0 kudos

Resolved! Importing System Workbench Project into STM32Cube IDE

I was able to import STMF4DISCOVERY_Ethernet-Phy-SystemWorkbench project into STM32Cube IDE. However, it seems the pathnames are a bit messed up. For example, it failed to find the make file. So is there a cookbook procedure to do this? Or am I b...

Is it possible to specify files/folders that should not be changed by the code generator? There is a plan to allow it?

Hi!We have a lot of problems with the automatic code generator. One of them. Sometimes we need to make changes to 'Drivers'/'Middlewares' and store them in our svn repository. If we include these libraries to our project via 'externals' and do code g...

RPerm.1 by Associate
  • 2117 Views
  • 4 replies
  • 0 kudos

Resolved! speed & code size stm32cubeIDE vs iar

hi i use of iar embedded workbench arm.But after seeing the ads and features of stm32cubeIDE, I used stm32cubeIDE for testing.There are two major drawbacks to stm32cubeIDE:1. The generated hex code is almost twice as long as iar(in flash memory).2- T...

kshin.111 by Associate III
  • 6146 Views
  • 5 replies
  • 0 kudos