STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32L4R9I-EVAL examples do not show up in target selector

I am running v1.6.1 of STM32CubeIDE.When target selector is run using File/New/STM32 Project it does not list any examples for STM32L4R9I-EVAL even though I can find them in the L4 repository.I ran Update TTarget Selector DB and no change.Is it possi...

RHerm.3 by Associate III
  • 1421 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeIDE (project importer) 1.6.0 Works well?

Hello.I upgraded STM32CubeIDE from 1.5.0 to 1.6.0.But, in my environment, STM32CubeIDE (project importer).exe doesn't work well.As a work-around, I executed same program of 1.5.0 and it works well.Does it work in other (language) environment?- OS: Wi...

BLUEnLIVE by Associate II
  • 2192 Views
  • 5 replies
  • 0 kudos

Hi, I just started to use STM32Cube IDE, and I was just workig on a project. I'm using a NUCLEO-F103RB board, but when I build the project (I'm using the default code) there's errors .

The errors are like this one:In file included from C:/Users/maria/STM32CubeIDE/workspace_1.3.0/led_*****/Drivers/CMSIS/Device/ST/STM32F1xx/Include/stm32f1xx.h:131,         from C:/Users/maria/STM32CubeIDE/workspace_1.3.0/led_*****/Drivers/STM32F1xx_H...

MGuim.2 by Associate
  • 3375 Views
  • 3 replies
  • 0 kudos

TIM6_DAC_IRQHandler Roution error.....?

Hai...,We have use to STM32F746IGT customboard and 7 inch displayCreat the code using CubeMX , TouchGFX, CubeIDE, While debugging HAL_Init(); and go to TIM6_DAC_IRQHandler (); and it's not retan,For TIM6 used to Timebase Soure: TIM6.Please give idea...

GMano.1 by Associate II
  • 1269 Views
  • 1 replies
  • 0 kudos

Resolved! 128 bit floating point not supported

Hi,I'm using STM32F767.​​I require the use of a 128 bit floating point in C and I couldn't find how to do so.I did a research on​line and I saw one suggestion to use the datatype "__float128"but the build failed due to "unknown datatype __float128"​I...

AKart.1 by Associate II
  • 2964 Views
  • 4 replies
  • 0 kudos