STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

NVIC ISERx registers address are wrong in STM32F446RE

I am using STM32F446RE. I am using the STM32CubeIDE. As STM32F446RE is Cortex-M4 based processor I have also gone through the M4 generic user guide and found that the range of NVIC_ISER0- NVIC_ISER7 is 0xE000E100- 0xE000E11C. But when I ran the code ...

0693W00000BaBsyQAF.png
PK by Associate II
  • 4729 Views
  • 12 replies
  • 0 kudos

In main.c I have #include <regex.h> and calls to regcomp and regexec. In the build output, I receive undefined reference to `regcomp'. Is it an error in the linker stage? What linker setting I should change?

MCU GCC Linker options are-mcpu=cortex-m3 -T"C:\Users\ssz\STM32CubeIDE\temp\edmr2\STM32F103VETX_FLASH.ld" --specs=nosys.specs -Wl,-Map="${BuildArtifactFileBaseName}.map" -Wl,--gc-sections -Wl,--verbose -static --specs=nano.specs -mfloat-abi=soft -mth...

Resolved! Debug CMake project with STM32CubeIDE

Hey, I'm using the latest Cube IDE and would like to Debug a Cmake Project.I'm using an Stm32F429 Disc Board for testing purposes.The Project Structure looks like this:myProjectSourceCodeapp (contains main() + ASM Startup Code + App Code)modulesSomeM...

0693W00000D08PGQAZ.png
JHeni.1 by Associate II
  • 4273 Views
  • 6 replies
  • 1 kudos

STM32CubeIDE 1.7.0 released

STM32CubeIDE 1.7.0 was released last week on st.com as well as an in-tool update patch.Caution: The in-tool update does not allow updating debug probe drivers and ST-LINK server tool. Full installer is required for this.What is new in 1.7.0?Target su...

HTTP Access Forbidden issues

I have the latest CubeIDE 1.7.0, but this phenomenon is exist on previous 1.6.1 too. Two computers, two IDE versions, the same phenomenons,It is not possible to download the TOUCHGFX pack via package manager.  When I am creating a new project, I get ...

0693W00000D0Z1QQAV.png 0693W00000D0Z1zQAF.png
Vuha by Associate II
  • 1251 Views
  • 1 replies
  • 0 kudos

Resolved! Issue when updating from the repository with version 1.7.0

I'm having the following error when reloading or updating from the repository:eclipse.buildId=Version 1.7.0java.version=11.0.10java.vendor=AdoptOpenJDKBootLoader constants: OS=macosx, ARCH=x86_64, WS=cocoa, NL=en_ITFramework arguments: -keyring /User...

MScac.11 by Associate II
  • 3003 Views
  • 6 replies
  • 0 kudos

Header files not showing up in project?

I'm using the NUCLEO H755ZI-Q project as part of the X-CUBE-AWS. But when I import my project, none of my header files or include folders appear in my project. In my included picture, I can find ethernetif.h on my computer and my project successfully...

0693W00000D0UWOQA3.png
MBlanco by Associate II
  • 1178 Views
  • 1 replies
  • 0 kudos

Resolved! How to compare Build Configurations

I've inherited a project that contains 10 build configurations. In the STM32CubeIde properties windows I cannot find any differences between a couple of the configurations. There are so many settings in various windows, tabs, etc. Instead of selec...

gsieb.1 by Associate II
  • 3113 Views
  • 3 replies
  • 0 kudos

Resolved! SWV not working with STM32L475

SWV trace and printf not works with my Discovery board STM32L475​VGT6 MCU. I am using using micro USB for connecting board with PC. How can I trace using SWV

SSIVA.1 by Associate
  • 1398 Views
  • 1 replies
  • 0 kudos