STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Why is sending WREN not setting my WEL bit?

I am using STM32H743 and trying to test my FRAM (FM25V20A) using SPI, I am able to read the device ID correctly but when I tried to write to the FRAM and read back I received zeros.I sent ULBPR and then WREN, when I read the status register using RDS...

Tee by Associate II
  • 2636 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F103 - Empty DMA buffer from ADC conversion

Hi Everyone, Probably a bit long question, but I try to give as much details as possible. Thank you in advance for your time!I am trying to trigger the ADC1 on a STM32F103C8T6 using a timer. The ADC uses the DMA and once the conversion is completed, ...

4ustenite by Associate II
  • 2634 Views
  • 3 replies
  • 0 kudos

I just want to try to write something in any particular flash memory address, using stm32cube ide, I am using these two functions for read and write as I mention above when I compile my code its compile successfully but I see my address 0x0807F800 blank

nt32_t Flash_Write_Data (uint32_t StartPageAddress, uint32_t *Data, uint16_t numberofwords){ static FLASH_EraseInitTypeDef EraseInitStruct; uint32_t PAGEError; int sofar=0;  /* Unlock the Flash to enable the flash control register access ************...

Amour.1 by Associate
  • 2255 Views
  • 3 replies
  • 0 kudos

Setup a fixed address for global variable

I am need to set a fixed address for global variable1. For several variables.2. For several const variable.I have tried to search information and examples on this matter, but was unsatisfied.I am using STM32F413VGTX, STM32CubeIDEThere is two ID files...

Ecohe by Associate II
  • 4320 Views
  • 3 replies
  • 0 kudos

Resolved! Can't find makefile

I am trying to run examples from the StmCubeF3 directory. I dbl click the project file and STM32CubeIDE comes up. When I try to build an error message states the makefile is not in the path. An ST document suggested moving my examples to a top leve...

John Hite by Associate III
  • 5431 Views
  • 6 replies
  • 0 kudos

Resolved! Which IDE to use for Nucleo boards?

I found nothing so far in product description or user manual for the Nucleo 144 (Nucleo-F303ZE) that specifies an IDE. When I tried to run an STM32CubeF3 example on the STM32CubeIDE it said the files were Nucleo type and needed to be converted. Is th...

John Hite by Associate III
  • 1377 Views
  • 2 replies
  • 0 kudos

Resolved! How to build Nucleo 144 projects?

Greetings,I just received a Nucleo-F303ZE aka Nucleo-144. The card says there would be code and examples on the NUCLEO-F303ZE page: https://www.st.com/en/evaluation-tools/nucleo-f303ze.htmlThat page said I might also like: STM32CubeF3. I downloaded t...

John Hite by Associate III
  • 3148 Views
  • 4 replies
  • 0 kudos