cancel
Showing results for 
Search instead for 
Did you mean: 

Why is sending WREN not setting my WEL bit?

Tee
Associate II

I am using STM32H743 and trying to test my FRAM (FM25V20A) using SPI, I am able to read the device ID correctly but when I tried to write to the FRAM and read back I received zeros.

I sent ULBPR and then WREN, when I read the status register using RDSR I received zeros which means that the WEL was not set.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Tee
Associate II

It turned out to be a silly mistake of using the wrong the SPI in the second part of the code.

View solution in original post

4 REPLIES 4
SKacp.1
Senior II

Hi,

I propose change in configuration for SPI1 Datasize from SPI_DATASIZE_4BIT to SPI_DATASIZE_8BIT.

Best Regards,

Slawek

It still isnt working, thank you anyway!

Hi,

Please see my code for write and read from FRAM FM25V10A

Best regards,

Slawek

void Write_UI_FR (uint16_t addr, uint16_t *data)
{
	uint8_t data_to_transmit[5];
 
	Enable_Write_FR();
 
	data_to_transmit[0] = OPCODE_WRITE;
	data_to_transmit[1] = addr >> 8;
	data_to_transmit[2] = addr;
	data_to_transmit[3] = *((uint8_t*)data);
	data_to_transmit[4] = *((uint8_t*)data+1);
 
	HAL_GPIO_WritePin(FR_CS_GPIO_Port, FR_CS_Pin, RESET);
	HAL_SPI_Transmit(&hspi2, &data_to_transmit[0], 5, 5);
	HAL_GPIO_WritePin(FR_CS_GPIO_Port, FR_CS_Pin, SET);
 
}
 
uint16_t Read_UI_FR (uint16_t addr, uint16_t *data)
{
	uint8_t data_recv[2];
	uint8_t data_to_transmit[4];
	uint16_t data_ret=0;
 
	Enable_Write_FR();
 
	data_to_transmit[0] = OPCODE_READ;
	data_to_transmit[1] = addr >> 8;
	data_to_transmit[2] = addr;
 
	HAL_GPIO_WritePin(FR_CS_GPIO_Port, FR_CS_Pin, RESET);
	HAL_SPI_Transmit(&hspi2, &data_to_transmit[0], 3, 5);
	HAL_SPI_Receive(&hspi2, &data_recv[0], 2, 5);
	HAL_GPIO_WritePin(FR_CS_GPIO_Port, FR_CS_Pin, SET);
 
	*((uint8_t*)data) = data_recv[0];
	*((uint8_t*)data+1) = data_recv[1];
 
	data_ret = (((uint16_t)(data_recv[0] << 8)) | data_recv[1]);
	return data_ret;
}
 
void Enable_Write_FR (void)
{
	opcodes_t code_func;
 
	code_func = OPCODE_WREN;
 
	HAL_GPIO_WritePin(FR_CS_GPIO_Port, FR_CS_Pin, RESET);
	HAL_SPI_Transmit(&hspi2, &code_func, 1, 5);
	HAL_GPIO_WritePin(FR_CS_GPIO_Port, FR_CS_Pin, SET);
 
}
 
void Disable_Write_FR (void)
{
	opcodes_t code_func;
 
	code_func = OPCODE_WRDI;
 
	HAL_GPIO_WritePin(FR_CS_GPIO_Port, FR_CS_Pin, RESET);
	HAL_SPI_Transmit(&hspi2, &code_func, 1, 5);
	HAL_GPIO_WritePin(FR_CS_GPIO_Port, FR_CS_Pin, SET);
 
}
 
typedef enum opcodes_e
{
  OPCODE_WREN   = 0b00000110,     /* Write Enable Latch */
  OPCODE_WRDI   = 0b00000100,     /* Reset Write Enable Latch */
  OPCODE_RDSR   = 0b00000101,     /* Read Status Register */
  OPCODE_WRSR   = 0b00000001,     /* Write Status Register */
  OPCODE_READ   = 0b00000011,     /* Read Memory */
  OPCODE_WRITE  = 0b00000010,     /* Write Memory */
  OPCODE_RDID   = 0b10011111      /* Read Device ID */
} opcodes_t;
 
 
 

Tee
Associate II

It turned out to be a silly mistake of using the wrong the SPI in the second part of the code.