STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! add arm library

hello everyoneI am a new researcher in the field and I need to develop a project with arm libraries to have some fft résultas I can find the library but i dont know how to make the project run, is there anyone who can help me?

JJuli.1 by Associate II
  • 2315 Views
  • 4 replies
  • 0 kudos

Resolved! How to export/duplicate my project from F030R8 to G070RB

hey,I Have a big Project on stm32 F030R8, and i would like to export/duplicateto a new board I have(G070RB).I am using Stm32CubeIDE, is there any magic option that it can do it by its self?Or I have to copy and past by hand (please no!).thanks in adv...

YShko.1 by Associate II
  • 1458 Views
  • 2 replies
  • 0 kudos

Can I use a USB C Breakout Board with a Nucleo board?

I'm working on a design for a custom keyboard, but I want to test as many components individually as I can before I start ordering parts. I have a Nucleo-G0B1RE (STM32G0B1), and I've carefully traced the PA11 [PA9] and PA12 [PA10] pins, and connected...

Comparing Nucleo-H743ZI2 and Nucleo-H745ZI-Q

I've written some code in STM32CubeIDE for the Nucleo-H743 which is simply toggling the board's LEDs and using the SPI channels to tx/rx with a few A/D converters. I've measured the loop's time to execute with a scope to be ~20us. I also have a Nucl...

CMcSh.1 by Associate II
  • 3843 Views
  • 6 replies
  • 0 kudos

Question on STM32CubeIDE and remote debugging

Hello, I am looking for some guidelines on how to make remote debugging possible with STM32CubeIDE running on Win10x64 and my STM32F070RB board connected to a Linux host.Everything works fine when the device is connected locally, but there is an opti...

elagano by Associate
  • 4537 Views
  • 5 replies
  • 2 kudos

Resolved! token pasting errors

I am trying to do token pasting to defined macros but it fails using this platform. main.h contains the definitions and the other file is my tokenpasting attempt getting errors but it works on netbeans

VNdir.1 by Associate II
  • 3521 Views
  • 2 replies
  • 0 kudos

How to see core utilization in stm32 cubeide?

I am using STM32L452RC for my project. I need to know the core utilization that is similar to how we see in the task manager. I need to know this, since I want to see the difference in the utilization with and without involving DMA. I need to verify ...

RAnan.3 by Associate III
  • 3372 Views
  • 5 replies
  • 0 kudos

STM32CubeIde freezes if a lot of data is SWV traced

HiI trace (or I try) uint32 variable (counter increased by the HOST USB interrupt) to trace MSC class problems (BTW many bugs in HAL USB Host library). I receive about 2 million traces in about 80 seconds. The problem is that eclipse if freezing and ...

0693W00000Y6kI4QAJ.jpg
pj_stm by Associate III
  • 2044 Views
  • 3 replies
  • 0 kudos

Resolved! How to debug mbed cpp program and make values visible

Hello. I am currently debugging an mbed cpp program in cubeIDE and trying to visualize the contents of variables. I was able to import from mbed to cubeIDE on my own. When I place a breakpoint on the variable I want to know about, I get the result [N...

0693W00000Y6tYgQAJ.png
hsanr.1 by Associate II
  • 2035 Views
  • 2 replies
  • 0 kudos