STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1557 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 590 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Build error

Hi, i have a STM32Cube project, that builds in stm32cubeide, however when porting it to VSCode extension and trying to build with cmake i get linker error saying: ../arm-none-eabi/lib/crt0.o: in function `_mainCRTStartup': undefined reference to 'mai...

JDydy.1 by Associate II
  • 2618 Views
  • 5 replies
  • 0 kudos

I have a problem on the debugging

i am using a STMCubeIDE v1.11.2 with windows 10 when i creat a new project it is working if i closed the IDE and open it again the problem below occureError in final launch sequence:Failed to execute MI command:target remote localhost:٦١٢٣٤Error mes...

0693W00000aJfQ3QAK.jpg
AAbde.8 by Associate II
  • 2557 Views
  • 5 replies
  • 0 kudos

STM32CubeIDE release configuration issue

Hello.Having an issue regarding Release configuration on STM32CubeIDE v1.12.0.I set up a new Build configuration "Release" with particular Debug level and Optimization level parameters set to None. When I build this configuration and try to Run, I ge...

xgn by Associate II
  • 1238 Views
  • 0 replies
  • 1 kudos

Resolved! My imported project build fails, how to fix it?

I have imported an STM32 project, created and debugged in the past using STM32CubeIDE. When I try to build this project in VSCode I see:Executing task: Build build task started...."C:\Program Files\CMake\bin\cmake.EXE" --build "D:/DataRoot/Projects/I...

SidPrice by Associate III
  • 6696 Views
  • 11 replies
  • 0 kudos

Any IoT node project on AWS for B-L475-IOT01A? (STM32CubeIDE)

I've been trying for weeks to find and build a project for B-L475-IOT01A that generates an IoT server on AWS, but I can't find anything for STM32CubeIDE that works properly, since I find a lot of failures when building the project when I try with exa...

DGarc.5 by Associate II
  • 1351 Views
  • 1 replies
  • 0 kudos

File tabs in STM32CubeIDE broken

I am using 2 separate workspaces, one which I created some years ago with an older version (workspace #1), and a newer one (workspace #2). Recently I imported an older project into workspace #1, and I am encountering the issue that the file tabs are ...

AWies.1 by Associate III
  • 2793 Views
  • 3 replies
  • 0 kudos