cancel
Showing results for 
Search instead for 
Did you mean: 

HardFault_Handler死循环 我下载了stm32cubeide很多版本1.5,1.11,1.12�?始化�?�,在输入主函数while�?,我�?试下载,�?��?�现都是第一步就�?�在 HardFault_Handler死循环,我试了试在keil上,结果正常,stm32cubeide这咋解决啊

Sss.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
KDJEM.1
ST Employee

Hello @Sss.1​  and welcome to the Community :),

Thanks to develop your posts in English so it helps us, and the users of our community understand your question and try to help you.

I've translated your question using a translation tool to increase the chances of getting you a reply from our experts and community members, since the majority interact in English.  

 Here is the translation of your post using Google translate:

HardFault_Handler infinite loop

I downloaded many versions of stm32cubeide 1.5, 1.11, and 1.12. After initialization, before entering the main function while, I tried to download, but found that the first step was stuck in the HardFault_Handler infinite loop. I tried it on keil, and the result was normal. How to solve stm32cubeide?

Could you please precise the STM32 product you are using?

Are you using an ST example?

I recommend you to follow this wiki.

Also, I advise you to start with an available example in the package.

I hope this helps you!

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.