STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1558 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 590 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! how to make keep ram value after software reset?

So i use to stm32cubeide & stm32h743zi. I want to create a variable that the system does not initailize even if the after software reset. just like __no_init in IAR.i follow this method. but i can't.https://atadiat.com/en/e-how-to-preserve-a-variable...

ikassma by Senior
  • 10568 Views
  • 7 replies
  • 2 kudos

Resolved! STM32CubeIDE HAL_I2C_ErrorCallback function does not work.

I'm using i2c interface to communicate with a eeprom memory, by dma. It's working, however, when I put a wrong address to write in the memory (to test the errors), I get as return HAL_ERROR, but the function HAL_I2C_ErrorCallback (that i implemented)...

Ade J.3 by Associate II
  • 5440 Views
  • 6 replies
  • 0 kudos

STM32CubeIDE Gitlab runner Docker image

Hi,I'm trying to setup a server (Ubuntu server 22.04) to build my STM32 projects.I installed a gitlab runner in docker container.I used this image xanderhendriks/stm32cubeide:7.0 and built my own using the newest version of stm32cubeide.however I'm r...

breakpoint not working

I have installed STM32CUBEIDE for software development.I am trying for internal debugger to debug my code and get the output on console but breakpoint not working.C code is not dependent on hardware.Please tell me setting in IDE so I can see output.

TSuta.1 by Associate
  • 1984 Views
  • 3 replies
  • 0 kudos