STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1559 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 592 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

CMSIS-Driver for DRIVER_Spi.h

Does anyone know how I include CMSIS-Driver's DRIVER_Spi.h library in CubeIDE? I was not able to find it installed by default. Is this library supported for STM32 Cube and if so, what is the CubeIDE way of adding it?

LMorr.3 by Senior II
  • 1930 Views
  • 2 replies
  • 0 kudos

TM Terminal plugin

I'd like to add the TM Terminal plugin to STMCubeIDE 1.12.0.I did add: After installation and restart the plugin didn't show up within the Show View List Box: Could somebody help me out it solving this problem?Thanks

0693W00000aJUEoQAO.png 0693W00000aJUG6QAO.png
MaSpieke by Associate
  • 2484 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE 1.12.1 wrong CDT update site

STM32CubeIDE version 1.12.1 (maybe other versions as well) has the wrong CDT update site configured by default. 1.12.1 uses CDT version 10.6 and Java 11, but CDT update site is configured as https://download.eclipse.org/tools/cdt/releases/latest/ whi...

Igor P. by Associate
  • 1865 Views
  • 1 replies
  • 2 kudos

Source File Initialization Errror

Hello,I am trying to control an AD5940 with STM32F4 SPI. I placed the AD5940.h and AD5940.c files in the main file but after debugging I got these errors. Do you have any idea how I can solve it? 12:37:26 **** Incremental Build of configuration Debug...

_legacyfs_online_stmicro_images_0693W00000dJqbcQAC.png
AE104 by Senior
  • 1332 Views
  • 0 replies
  • 0 kudos

Resolved! [SOLVED] Sprintf with floating point number crashing into hard fault on STM32L476, working fine with STM32F091

I'm trying to use this C code#include <stdio.h>     char arr[50]; int var_int; float var_float;   int main (void) { while (1) { var_int++; sprintf (arr,"RES 1 %d",var_int); var_float = var_float + 0.1; sprintf (arr,"RES2 %d %f",var_int,var_float...

0693W00000GYFKSQA5.png 0693W00000GYFJyQAP.png 0693W00000GYFMYQA5.png

how can i manually include std peripheral libraries to my project as i add the directory path to the compiler and still getting "no such folder or directory"

Right-click on your project in the Project Explorer and select "Properties" from the context menu.In the Properties dialog box, expand "C/C++ General" and select "Paths and Symbols".In the "Paths and Symbols" dialog box, select the "Includes" tab.Cli...

amusa.1 by Associate
  • 1108 Views
  • 0 replies
  • 0 kudos