STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1298 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 525 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! IOC File Not Displaying Diagram

I upgraded STM32Cube IDE to 1.12.0, and now when I double-click the IOC file, it just displays a text file, not the processor pin / configuration diagrams, etc.  I tried closing and re-opening the project(s) and closing and re-opening CubeIDE.  No ch...

RHJ by Associate II
  • 671 Views
  • 5 replies
  • 0 kudos

Resolved! Apple Mac M4 and STMCubeIDE

2.0 of STMCubeIDE loads but is missing the New Project 'wizard' of 1.15:2.0 only allows a blank project to be created, but missing the graphic of the uP.1.15 allows wizard to run but then fails at the last step with error message something to do with...

J_MPU by Associate
  • 765 Views
  • 3 replies
  • 2 kudos

Build a STM32CubeIDE project via command line

I have a STM32 project created for STM32H757 which has dual core CPU. The directory structure is look like this:I wanted to build this project using command line in my ubutnu machine. I have tried with this command:$ <INSTALLTION_DIRECTORY>/st/stm32c...

virendra_dalal_0-1763558849799.png

Still facing STM32Cube option greyed out

Hi all,I'm experiencing the exact same issue described in this thread (https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-stm32cube-project-creation-issue/td-p/823125) with STM32CubeIDE v1.19.0 on Windows. After selecting a target MCU during ...